WedmBasedGeomBuilder Class¶
-
class
NXOpen.CAM.
WedmBasedGeomBuilder
¶ Bases:
NXOpen.CAM.ParamBuilder
Represents a WedmBasedGeom Builder
To create a new instance of this class, use
NXOpen.CAM.NCGroupCollection.CreateWedmBasedGeomBuilder
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
BackburnPasses | Returns or sets the Backburn Passes |
CustomBoundaryDataList | Returns the Custom Boundary Data List |
CutDirection | Returns or sets the Cut Direction |
CutoffDistance | Returns or sets the Cutoff Distance |
CutoffFlag | Returns or sets the Cutoff Flag |
CutoffStock | Returns or sets the Cutoff Stock |
CycleEvent | Returns the cycle event |
CycleTable | Returns the cycle |
FinishPasses | Returns or sets the Finish Passes |
FromPoint | Returns or sets the From Point |
FromPointStatus | Returns or sets the From Point Status |
FromPointToolAxis | Returns or sets the From Point Tool Axis |
GoHomePoint | Returns or sets the Go Home Point |
GoHomePointStatus | Returns or sets the Go Home Point Status |
GoHomePointToolAxis | Returns or sets the Go Home Point Tool Axis |
Intol | Returns or sets the intol value |
LayoutCiBuilder | Returns the Save Layer/Layout builder |
LeadInPoint | Returns or sets the Lead In Point |
LeadInPointStatus | Returns or sets the Lead In Point Status |
LeadOutPointStatus | Returns or sets the Lead Out Point Status |
LowerPlane | Returns or sets the Lower Plane |
NumTabs | Returns or sets the Tab Points |
OptimizationMethod | Returns or sets the optim method |
Outtol | Returns or sets the outtol value |
RegionMethod | Returns or sets the Tab Points Region Method |
RetractPoint | Returns or sets the Retract Point |
RetractPointStatus | Returns or sets the Retract Point Status |
RetractPointToolAxis | Returns or sets the Retract Point Tool Axis |
RoughPasses | Returns or sets the Rough Passes |
SmoothLeadinDistance | Returns or sets the Smooth Leadin Distance |
SmoothLeadinFlag | Returns or sets the Smooth Leadin Flag |
SmoothLeadoutDistance | Returns or sets the Smooth Leadout Distance |
SmoothLeadoutFlag | Returns or sets the Smooth Leadout Flag |
StepoverBuilder | Returns the Stepover builder |
StopPointDistance | Returns or sets the Stop Point Distance |
StopPointFlag | Returns or sets the Stop Point Flag |
StopPointType | Returns or sets the Stop Point Type |
Tag | Returns the Tag for this object. |
ThreadHolePoint | Returns or sets the Thread Hole Point |
ThreadHolePointStatus | Returns or sets the Thread Hole Point Status |
ThreadHolePointToolAxis | Returns or sets the Thread Hole Point Tool Axis |
UpperPlane | Returns or sets the Upper Plane |
WireDiameter | Returns or sets the Wire Diameter |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
BackburnPasses¶
-
WedmBasedGeomBuilder.
BackburnPasses
¶ Returns or sets the Backburn Passes
-------------------------------------
Getter Method
Signature
BackburnPasses()
Returns: the Backburn Passes Return type: int New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
BackburnPasses(backburnPasses)
Parameters: backburnPasses (int) – the Backburn Passes New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
CustomBoundaryDataList¶
-
WedmBasedGeomBuilder.
CustomBoundaryDataList
¶ Returns the Custom Boundary Data List
-------------------------------------
Getter Method
Signature
CustomBoundaryDataList()
Returns: the Custom Boundary Data Return type: NXOpen.CAM.WedmCustomBoundaryDataBuilderList
New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
CutDirection¶
-
WedmBasedGeomBuilder.
CutDirection
¶ Returns or sets the Cut Direction
-------------------------------------
Getter Method
Signature
CutDirection()
Returns: the Cut Direction Return type: int New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
CutDirection(cutDirection)
Parameters: cutDirection (int) – the Cut Direction New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
CutoffDistance¶
-
WedmBasedGeomBuilder.
CutoffDistance
¶ Returns or sets the Cutoff Distance
-------------------------------------
Getter Method
Signature
CutoffDistance()
Returns: the Cutoff Distance Return type: float New in version NX5.0.1.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
CutoffDistance(cutoffDistance)
Parameters: cutoffDistance (float) – the Cutoff Distance New in version NX5.0.1.
License requirements: cam_base (“CAM BASE”)
CutoffFlag¶
-
WedmBasedGeomBuilder.
CutoffFlag
¶ Returns or sets the Cutoff Flag
-------------------------------------
Getter Method
Signature
CutoffFlag()
Returns: the Cutoff Flag Return type: int New in version NX5.0.1.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
CutoffFlag(cutoffFlag)
Parameters: cutoffFlag (int) – the Cutoff Flag New in version NX5.0.1.
License requirements: cam_base (“CAM BASE”)
CutoffStock¶
-
WedmBasedGeomBuilder.
CutoffStock
¶ Returns or sets the Cutoff Stock
-------------------------------------
Getter Method
Signature
CutoffStock()
Returns: the Cutoff Stock Return type: float New in version NX5.0.1.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
CutoffStock(cutoffStock)
Parameters: cutoffStock (float) – the Cutoff Stock New in version NX5.0.1.
License requirements: cam_base (“CAM BASE”)
FinishPasses¶
-
WedmBasedGeomBuilder.
FinishPasses
¶ Returns or sets the Finish Passes
-------------------------------------
Getter Method
Signature
FinishPasses()
Returns: the Finish Passes Return type: int New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
FinishPasses(finishPasses)
Parameters: finishPasses (int) – the Finish Passes New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
FromPoint¶
-
WedmBasedGeomBuilder.
FromPoint
¶ Returns or sets the From Point
-------------------------------------
Getter Method
Signature
FromPoint()
Returns: the From Point Return type: NXOpen.NXObject
New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
FromPoint(point)
Parameters: point ( NXOpen.NXObject
) – the From PointNew in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
FromPointStatus¶
-
WedmBasedGeomBuilder.
FromPointStatus
¶ Returns or sets the From Point Status
-------------------------------------
Getter Method
Signature
FromPointStatus()
Returns: the From Point Status Return type: int New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
FromPointStatus(status)
Parameters: status (int) – the From Point Status New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
FromPointToolAxis¶
-
WedmBasedGeomBuilder.
FromPointToolAxis
¶ Returns or sets the From Point Tool Axis
-------------------------------------
Getter Method
Signature
FromPointToolAxis()
Returns: the From Point Tool Axis Return type: NXOpen.NXObject
New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
FromPointToolAxis(toolAxis)
Parameters: toolAxis ( NXOpen.NXObject
) – the From Point Tool AxisNew in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
GoHomePoint¶
-
WedmBasedGeomBuilder.
GoHomePoint
¶ Returns or sets the Go Home Point
-------------------------------------
Getter Method
Signature
GoHomePoint()
Returns: the Go Home Point Return type: NXOpen.NXObject
New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
GoHomePoint(point)
Parameters: point ( NXOpen.NXObject
) – the Go Home PointNew in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
GoHomePointStatus¶
-
WedmBasedGeomBuilder.
GoHomePointStatus
¶ Returns or sets the Go Home Point Status
-------------------------------------
Getter Method
Signature
GoHomePointStatus()
Returns: the Go Home Point Status Return type: int New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
GoHomePointStatus(status)
Parameters: status (int) – the Go Home Point Status New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
GoHomePointToolAxis¶
-
WedmBasedGeomBuilder.
GoHomePointToolAxis
¶ Returns or sets the Go Home Point Tool Axis
-------------------------------------
Getter Method
Signature
GoHomePointToolAxis()
Returns: the Go Home Point Tool Axis Return type: NXOpen.NXObject
New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
GoHomePointToolAxis(toolAxis)
Parameters: toolAxis ( NXOpen.NXObject
) – the Go Home Point Tool AxisNew in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
Intol¶
-
WedmBasedGeomBuilder.
Intol
¶ Returns or sets the intol value
-------------------------------------
Getter Method
Signature
Intol()
Returns: the intol value Return type: float New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
Intol(intol)
Parameters: intol (float) – the intol value New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
LayoutCiBuilder¶
-
WedmBasedGeomBuilder.
LayoutCiBuilder
¶ Returns the Save Layer/Layout builder
-------------------------------------
Getter Method
Signature
LayoutCiBuilder()
Returns: the save layer/layout builder Return type: NXOpen.CAM.LayoutCiBuilder
New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
LeadInPoint¶
-
WedmBasedGeomBuilder.
LeadInPoint
¶ Returns or sets the Lead In Point
-------------------------------------
Getter Method
Signature
LeadInPoint()
Returns: the Lead In Point Return type: NXOpen.NXObject
New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
LeadInPoint(point)
Parameters: point ( NXOpen.NXObject
) – the Lead In PointNew in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
LeadInPointStatus¶
-
WedmBasedGeomBuilder.
LeadInPointStatus
¶ Returns or sets the Lead In Point Status
-------------------------------------
Getter Method
Signature
LeadInPointStatus()
Returns: the Lead In Point Status Return type: int New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
LeadInPointStatus(status)
Parameters: status (int) – the Lead In Point Status New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
LeadOutPointStatus¶
-
WedmBasedGeomBuilder.
LeadOutPointStatus
¶ Returns or sets the Lead Out Point Status
-------------------------------------
Getter Method
Signature
LeadOutPointStatus()
Returns: the Lead Out Point Status Return type: int New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
LeadOutPointStatus(status)
Parameters: status (int) – the Lead Out Point Status New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
LowerPlane¶
-
WedmBasedGeomBuilder.
LowerPlane
¶ Returns or sets the Lower Plane
-------------------------------------
Getter Method
Signature
LowerPlane()
Returns: the Lower Plane Return type: float New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
LowerPlane(lowerPlane)
Parameters: lowerPlane (float) – the Lower Plane New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
NumTabs¶
-
WedmBasedGeomBuilder.
NumTabs
¶ Returns or sets the Tab Points
-------------------------------------
Getter Method
Signature
NumTabs()
Returns: the Num Tabs Return type: int New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
NumTabs(numTabs)
Parameters: numTabs (int) – the Num Tabs New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
Outtol¶
-
WedmBasedGeomBuilder.
Outtol
¶ Returns or sets the outtol value
-------------------------------------
Getter Method
Signature
Outtol()
Returns: the intol value Return type: float New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
Outtol(outtol)
Parameters: outtol (float) – the intol value New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
RegionMethod¶
-
WedmBasedGeomBuilder.
RegionMethod
¶ Returns or sets the Tab Points Region Method
-------------------------------------
Getter Method
Signature
RegionMethod()
Returns: the Tab Points Region Method Return type: int New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
RegionMethod(regionMethod)
Parameters: regionMethod (int) – the Tab Points Region Method New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
RetractPoint¶
-
WedmBasedGeomBuilder.
RetractPoint
¶ Returns or sets the Retract Point
-------------------------------------
Getter Method
Signature
RetractPoint()
Returns: the Retract Point Return type: NXOpen.NXObject
New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
RetractPoint(point)
Parameters: point ( NXOpen.NXObject
) – the Retract PointNew in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
RetractPointStatus¶
-
WedmBasedGeomBuilder.
RetractPointStatus
¶ Returns or sets the Retract Point Status
-------------------------------------
Getter Method
Signature
RetractPointStatus()
Returns: the Retract Point Status Return type: int New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
RetractPointStatus(status)
Parameters: status (int) – the Retract Point Status New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
RetractPointToolAxis¶
-
WedmBasedGeomBuilder.
RetractPointToolAxis
¶ Returns or sets the Retract Point Tool Axis
-------------------------------------
Getter Method
Signature
RetractPointToolAxis()
Returns: the Retract Point Tool Axis Return type: NXOpen.NXObject
New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
RetractPointToolAxis(toolAxis)
Parameters: toolAxis ( NXOpen.NXObject
) – the Retract Point Tool AxisNew in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
RoughPasses¶
-
WedmBasedGeomBuilder.
RoughPasses
¶ Returns or sets the Rough Passes
-------------------------------------
Getter Method
Signature
RoughPasses()
Returns: the Rough Passes Return type: int New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
RoughPasses(roughPasses)
Parameters: roughPasses (int) – the Rough Passes New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
SmoothLeadinDistance¶
-
WedmBasedGeomBuilder.
SmoothLeadinDistance
¶ Returns or sets the Smooth Leadin Distance
-------------------------------------
Getter Method
Signature
SmoothLeadinDistance()
Returns: the Smooth Leadin Distance Return type: float New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
SmoothLeadinDistance(leadInDistance)
Parameters: leadInDistance (float) – the Smooth Leadin Distance New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
SmoothLeadinFlag¶
-
WedmBasedGeomBuilder.
SmoothLeadinFlag
¶ Returns or sets the Smooth Leadin Flag
-------------------------------------
Getter Method
Signature
SmoothLeadinFlag()
Returns: the Smooth Leadin Flag Return type: int New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
SmoothLeadinFlag(leadInFlag)
Parameters: leadInFlag (int) – the Smooth Leadin Flag New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
SmoothLeadoutDistance¶
-
WedmBasedGeomBuilder.
SmoothLeadoutDistance
¶ Returns or sets the Smooth Leadout Distance
-------------------------------------
Getter Method
Signature
SmoothLeadoutDistance()
Returns: the Smooth Leadout Distance Return type: float New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
SmoothLeadoutDistance(leadOutDistance)
Parameters: leadOutDistance (float) – the Smooth Leadout Distance New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
SmoothLeadoutFlag¶
-
WedmBasedGeomBuilder.
SmoothLeadoutFlag
¶ Returns or sets the Smooth Leadout Flag
-------------------------------------
Getter Method
Signature
SmoothLeadoutFlag()
Returns: the Smooth Leadout Flag Return type: int New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
SmoothLeadoutFlag(leadOutFlag)
Parameters: leadOutFlag (int) – the Smooth Leadout Flag New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
StepoverBuilder¶
-
WedmBasedGeomBuilder.
StepoverBuilder
¶ Returns the Stepover builder
-------------------------------------
Getter Method
Signature
StepoverBuilder()
Returns: the Stepover Builder Return type: NXOpen.CAM.StepoverBuilder
New in version NX6.0.0.
License requirements: None.
StopPointDistance¶
-
WedmBasedGeomBuilder.
StopPointDistance
¶ Returns or sets the Stop Point Distance
-------------------------------------
Getter Method
Signature
StopPointDistance()
Returns: the Stop Point Distance Return type: float New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
StopPointDistance(stopPointDistance)
Parameters: stopPointDistance (float) – the Stop Point Distance New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
StopPointFlag¶
-
WedmBasedGeomBuilder.
StopPointFlag
¶ Returns or sets the Stop Point Flag
-------------------------------------
Getter Method
Signature
StopPointFlag()
Returns: the Stop Point Flag Return type: int New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
StopPointFlag(stopPointFlag)
Parameters: stopPointFlag (int) – the Stop Point Flag New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
StopPointType¶
-
WedmBasedGeomBuilder.
StopPointType
¶ Returns or sets the Stop Point Type
-------------------------------------
Getter Method
Signature
StopPointType()
Returns: the Stop Point Type Return type: int New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
StopPointType(stopPointType)
Parameters: stopPointType (int) – the Stop Point Type New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
ThreadHolePoint¶
-
WedmBasedGeomBuilder.
ThreadHolePoint
¶ Returns or sets the Thread Hole Point
-------------------------------------
Getter Method
Signature
ThreadHolePoint()
Returns: the Thread Hole Point Return type: NXOpen.NXObject
New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
ThreadHolePoint(point)
Parameters: point ( NXOpen.NXObject
) – the Thread Hole PointNew in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
ThreadHolePointStatus¶
-
WedmBasedGeomBuilder.
ThreadHolePointStatus
¶ Returns or sets the Thread Hole Point Status
-------------------------------------
Getter Method
Signature
ThreadHolePointStatus()
Returns: the Thread Hole Point Status Return type: int New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
ThreadHolePointStatus(status)
Parameters: status (int) – the Thread Hole Point Status New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
ThreadHolePointToolAxis¶
-
WedmBasedGeomBuilder.
ThreadHolePointToolAxis
¶ Returns or sets the Thread Hole Point Tool Axis
-------------------------------------
Getter Method
Signature
ThreadHolePointToolAxis()
Returns: the Thread Hole Point Tool Axis Return type: NXOpen.NXObject
New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
ThreadHolePointToolAxis(toolAxis)
Parameters: toolAxis ( NXOpen.NXObject
) – the Thread Hole Point Tool AxisNew in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
UpperPlane¶
-
WedmBasedGeomBuilder.
UpperPlane
¶ Returns or sets the Upper Plane
-------------------------------------
Getter Method
Signature
UpperPlane()
Returns: the Upper Plane Return type: float New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
UpperPlane(upperPlane)
Parameters: upperPlane (float) – the Upper Plane New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
WireDiameter¶
-
WedmBasedGeomBuilder.
WireDiameter
¶ Returns or sets the Wire Diameter
-------------------------------------
Getter Method
Signature
WireDiameter()
Returns: the Wire Diameter Return type: float New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
WireDiameter(wireDiameter)
Parameters: wireDiameter (float) – the Wire Diameter New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
Method Detail¶
Validate¶
-
WedmBasedGeomBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.