WedmArcOutputTypeCiBuilder Class¶
-
class
NXOpen.CAM.
WedmArcOutputTypeCiBuilder
¶ Bases:
NXOpen.TaggedObject
Represents a WedmArcOutputTypeCiBuilder
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
OutputType | Returns or sets the Motion Output Type |
Tag | Returns the Tag for this object. |
Methods¶
Enumerations¶
WedmArcOutputTypeCiBuilderOutputTypes Enumeration | Available types for output |
Property Detail¶
OutputType¶
-
WedmArcOutputTypeCiBuilder.
OutputType
¶ Returns or sets the Motion Output Type
-------------------------------------
Getter Method
Signature
OutputType()
Returns: the motion output type Return type: NXOpen.CAM.WedmArcOutputTypeCiBuilderOutputTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OutputType(outputType)
Parameters: outputType ( NXOpen.CAM.WedmArcOutputTypeCiBuilderOutputTypes
) – the motion output typeNew in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)