VerticalPosition Class¶
-
class
NXOpen.CAM.
VerticalPosition
¶ Bases:
NXOpen.TaggedObject
Represents a VerticalPosition Builder
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
Distance | Returns or sets the distance |
OffsetType | Returns or sets the offset type |
Tag | Returns the Tag for this object. |
TeethNumber | Returns or sets the teeth number |
Methods¶
Enumerations¶
VerticalPositionOffsetTypes Enumeration | offset options |
Property Detail¶
Distance¶
-
VerticalPosition.
Distance
¶ Returns or sets the distance
-------------------------------------
Getter Method
Signature
Distance()
Returns: the distance Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Distance(distance)
Parameters: distance (float) – the distance New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
OffsetType¶
-
VerticalPosition.
OffsetType
¶ Returns or sets the offset type
-------------------------------------
Getter Method
Signature
OffsetType()
Returns: the offset type Return type: NXOpen.CAM.VerticalPositionOffsetTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OffsetType(newValue)
Parameters: newValue ( NXOpen.CAM.VerticalPositionOffsetTypes
) – the offset typeNew in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
TeethNumber¶
-
VerticalPosition.
TeethNumber
¶ Returns or sets the teeth number
-------------------------------------
Getter Method
Signature
TeethNumber()
Returns: the teeth number Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TeethNumber(teethNumber)
Parameters: teethNumber (float) – the teeth number New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)