TurnToolBuilderThicknessTypes Enumeration¶
NXOpen.CAM.TurnToolBuilder.ThicknessTypes is an alias for NXOpen.CAM.TurnToolBuilderThicknessTypes
-
class
NXOpen.CAM.
TurnToolBuilderThicknessTypes
¶ Bases:
object
the available thickness types
Enum Members
Enum Member Enum Member Description Thickness01 Thickness: 01ThicknessT1 Thickness: T1Thickness02 Thickness: 02ThicknessT2 Thickness: T2Thickness03 Thickness: 03ThicknessT3 Thickness: T3Thickness04 Thickness: 04Thickness05 Thickness: 05Thickness06 Thickness: 06Thickness07 Thickness: 07Thickness09 Thickness: 09Thickness11 Thickness: 11Thickness12 Thickness: 12ThicknessUserDefined Thickness: User defined-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-