TurnToolBuilderInsertShapes Enumeration¶
NXOpen.CAM.TurnToolBuilder.InsertShapes is an alias for NXOpen.CAM.TurnToolBuilderInsertShapes
-
class
NXOpen.CAM.
TurnToolBuilderInsertShapes
¶ Bases:
object
the available insert shapes
Enum Members
Enum Member Enum Member Description Parallelogram85 Insert shape: Parallelogram 85Parallelogram82 Insert shape: Parallelogram 82Diamond80 Insert shape: Diamond 80Diamond100 Insert shape: Diamond 100Diamond55 Insert shape: Diamond 55Diamond75 Insert shape: Diamond 75Hexagon Insert shape: HexagonParallelogram55 Insert shape: Parallelogram 55Rectangle Insert shape: RectangleDiamond86 Insert shape: Diamond 86Octagon Insert shape: OctagonPentagon Insert shape: PentagonRound Insert shape: RoundSquare Insert shape: SquareTriangle Insert shape: TriangleDiamond35 Insert shape: Diamond 35Trigon Insert shape: TrigonUser Insert shape: User defined-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-