TurnThreadFinishPassesBuilder Class¶
-
class
NXOpen.CAM.
TurnThreadFinishPassesBuilder
¶ Bases:
NXOpen.TaggedObject
Represents a TurnThreadFinishPasses Builder
New in version NX6.0.0.
Methods¶
Method | Description |
---|---|
Add | Create a new finish passes item. |
Delete | Delete an existing finish passes item |
Modify | Modify an existing finish passes item |
Method Detail¶
Add¶
-
TurnThreadFinishPassesBuilder.
Add
¶ Create a new finish passes item.
Add at the end of the current List.
Signature
Add(numberOfPasses, increment)
Parameters: - numberOfPasses (int) – the number of passes
- increment (float) – the increment
New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
Delete¶
-
TurnThreadFinishPassesBuilder.
Delete
¶ Delete an existing finish passes item
Signature
Delete(nodeIndex)
Parameters: nodeIndex (int) – the selected entry index New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
Modify¶
-
TurnThreadFinishPassesBuilder.
Modify
¶ Modify an existing finish passes item
Signature
Modify(index, numberOfPasses, increment)
Parameters: - index (int) – the index of modified item
- numberOfPasses (int) – the number of passes
- increment (float) – the increment
New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)