TurnRoughFinishLocalReturnBuilderModeTypes Enumeration¶
NXOpen.CAM.TurnRoughFinishLocalReturnBuilder.ModeTypes is an alias for NXOpen.CAM.TurnRoughFinishLocalReturnBuilderModeTypes
-
class
NXOpen.CAM.
TurnRoughFinishLocalReturnBuilderModeTypes
¶ Bases:
object
The local return type options
New in version NX6.0.0.
Enum Members
Enum Member Enum Member Description None Local Return: NoneDistance Local Return: DistanceTime Local Return: TimeNumberOfPasses Local Return: Number of PassesNumberOfCuts Local Return: Number of CutsNumberOfLevels Local Return: Number of Levels-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-