TurnOrientWcs Class¶
-
class
NXOpen.CAM.
TurnOrientWcs
¶ Bases:
NXOpen.TaggedObject
Represents an Turn Orient Wcs Builder
This is an abstract class, and cannot be instantiated.
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
Tag | Returns the Tag for this object. |
WcsOffset | Returns or sets the offset of the WCS origin |
XcMapping | Returns or sets the XC mapping |
YcMapping | Returns or sets the YC mapping |
Methods¶
Enumerations¶
TurnOrientWcsXcMappingTypes Enumeration | the XC mapping types |
TurnOrientWcsYcMappingTypes Enumeration | the YC mapping types |
Property Detail¶
WcsOffset¶
-
TurnOrientWcs.
WcsOffset
¶ Returns or sets the offset of the WCS origin
-------------------------------------
Getter Method
Signature
WcsOffset()
Returns: Offset of the WCS origin along the spindle axis Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
WcsOffset(wcsOffset)
Parameters: wcsOffset (float) – Offset of the WCS origin along the spindle axis New in version NX7.5.0.
License requirements: None.
XcMapping¶
-
TurnOrientWcs.
XcMapping
¶ Returns or sets the XC mapping
-------------------------------------
Getter Method
Signature
XcMapping()
Returns: XC mapping to an MCS axis Return type: NXOpen.CAM.TurnOrientWcsXcMappingTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
XcMapping(xcMapping)
Parameters: xcMapping ( NXOpen.CAM.TurnOrientWcsXcMappingTypes
) – XC mapping to an MCS axisNew in version NX7.5.0.
License requirements: None.
YcMapping¶
-
TurnOrientWcs.
YcMapping
¶ Returns or sets the YC mapping
-------------------------------------
Getter Method
Signature
YcMapping()
Returns: YC mapping to an MCS axis Return type: NXOpen.CAM.TurnOrientWcsYcMappingTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
YcMapping(ycMapping)
Parameters: ycMapping ( NXOpen.CAM.TurnOrientWcsYcMappingTypes
) – YC mapping to an MCS axisNew in version NX7.5.0.
License requirements: None.