TurnMethodBuilder Class¶
-
class
NXOpen.CAM.
TurnMethodBuilder
¶ Bases:
NXOpen.CAM.MethodBuilder
Represents a Turn Method Builder
To create a new instance of this class, use
NXOpen.CAM.NCGroupCollection.CreateTurnMethodBuilder
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
CutParameters | Returns the cut parameter object |
CycleEvent | Returns the cycle event |
CycleTable | Returns the cycle |
Description | Returns or sets the description |
EndUdeSet | Returns the end ude set |
FaceStockBuilder | Returns the face stock builder (inheritable double) |
FeedsBuilder | Returns the feeds builder |
OptimizationMethod | Returns or sets the optim method |
PaintDisplay | Returns the sub builder for paint display |
PathDisplay | Returns the sub builder for path display |
PathDisplayColors | Returns the sub builder for path display colors |
RadStockBuilder | Returns the radial stock builder (inheritable double) |
SilhouDisplay | Returns the sub builder for silhou display |
StartUdeSet | Returns the start ude set |
StockPartBuilder | Returns the part stock builder (inheritable double) |
Tag | Returns the Tag for this object. |
ToolDisplay | Returns the sub builder for tool display |
TurnEngRetMinDistBuilder | Returns the minimum engage/retract distance builder (inheritable double) |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetCutMethod | Get cut method @return |
GetObject | Returns the object currently being edited by this builder. |
GetTurnDisplCollTog | Get the display collisions value @return the display collisions value |
SetCutMethod | Set cut method |
SetTurnDisplCollTog | Set the display collisions value |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
FaceStockBuilder¶
-
TurnMethodBuilder.
FaceStockBuilder
¶ Returns the face stock builder (inheritable double)
-------------------------------------
Getter Method
Signature
FaceStockBuilder()
Returns: The face stock builder Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
FeedsBuilder¶
-
TurnMethodBuilder.
FeedsBuilder
¶ Returns the feeds builder
-------------------------------------
Getter Method
Signature
FeedsBuilder()
Returns: the feeds builder Return type: NXOpen.CAM.FeedsTurnBuilder
New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
RadStockBuilder¶
-
TurnMethodBuilder.
RadStockBuilder
¶ Returns the radial stock builder (inheritable double)
-------------------------------------
Getter Method
Signature
RadStockBuilder()
Returns: The radial stock builder Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
StockPartBuilder¶
-
TurnMethodBuilder.
StockPartBuilder
¶ Returns the part stock builder (inheritable double)
-------------------------------------
Getter Method
Signature
StockPartBuilder()
Returns: The stock part builder Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
TurnEngRetMinDistBuilder¶
-
TurnMethodBuilder.
TurnEngRetMinDistBuilder
¶ Returns the minimum engage/retract distance builder (inheritable double)
-------------------------------------
Getter Method
Signature
TurnEngRetMinDistBuilder()
Returns: The minimum engage/retract distance builder Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
Method Detail¶
GetTurnDisplCollTog¶
-
TurnMethodBuilder.
GetTurnDisplCollTog
¶ Get the display collisions value
Signature
GetTurnDisplCollTog()
Returns: the display collisions value Return type: int New in version NX5.0.0.
License requirements: None.
SetTurnDisplCollTog¶
-
TurnMethodBuilder.
SetTurnDisplCollTog
¶ Set the display collisions value
Signature
SetTurnDisplCollTog(displayValue)
Parameters: displayValue (int) – the display collisions value value New in version NX5.0.0.
License requirements: None.
Validate¶
-
TurnMethodBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.