TurnGrooveCornerControlReliefPlungeTypes Enumeration¶
NXOpen.CAM.TurnGrooveCornerControl.ReliefPlungeTypes is an alias for NXOpen.CAM.TurnGrooveCornerControlReliefPlungeTypes
-
class
NXOpen.CAM.
TurnGrooveCornerControlReliefPlungeTypes
¶ Bases:
object
the Groove Corner Control relief plunge types
New in version NX9.0.0.
Enum Members
Enum Member Enum Member Description None Groove Corner Control Relief Plunge Type is None.Depth Groove Corner Control Relief Plunge Type is Depth.WallDepth Groove Corner Control Relief Plunge Type is Wall Depth.Distance Groove Corner Control Relief Plunge Type is Distance.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-