TurnCornerControl Class¶
-
class
NXOpen.CAM.
TurnCornerControl
¶ Bases:
NXOpen.TaggedObject
Represents a first plunge ja
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
MinAngle | Returns or sets the minimum angle |
Radius | Returns or sets the Corner Control radius |
Tag | Returns the Tag for this object. |
Type | Returns or sets the Corner Control Types |
Methods¶
Enumerations¶
TurnCornerControlTypes Enumeration | the Corner Control Types options |
Property Detail¶
MinAngle¶
-
TurnCornerControl.
MinAngle
¶ Returns or sets the minimum angle
-------------------------------------
Getter Method
Signature
MinAngle()
Returns: Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MinAngle(doubleValue)
Parameters: doubleValue (float) – the the minimum angle New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
Radius¶
-
TurnCornerControl.
Radius
¶ Returns or sets the Corner Control radius
-------------------------------------
Getter Method
Signature
Radius()
Returns: Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Radius(doubleValue)
Parameters: doubleValue (float) – New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
Type¶
-
TurnCornerControl.
Type
¶ Returns or sets the Corner Control Types
-------------------------------------
Getter Method
Signature
Type()
Returns: the Corner Control Types Return type: NXOpen.CAM.TurnCornerControlTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type(cornerType)
Parameters: cornerType ( NXOpen.CAM.TurnCornerControlTypes
) –New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)