TurnAvoidanceReturnBuilderReturnPointMotionTypes Enumeration¶
NXOpen.CAM.TurnAvoidanceReturnBuilder.ReturnPointMotionTypes is an alias for NXOpen.CAM.TurnAvoidanceReturnBuilderReturnPointMotionTypes
-
class
NXOpen.CAM.
TurnAvoidanceReturnBuilderReturnPointMotionTypes
¶ Bases:
object
the return point motion type options
New in version NX6.0.0.
Enum Members
Enum Member Enum Member Description None Point is inactive.Automatic Motion type: Automatic to point.Direct Motion type: Direct to point.RadialThenAxial Motion type: Radial then axial to point.AxialThenRadial Motion type: Axial then axial to point.ClearRadialThenDirect Motion type: Radial to clearance plane then direct to point.ClearAxialThenDirect Motion type: Axial to clearance plane then direct to point.ClearRadialOnly Motion type: Radial to clearance plane only (no motion to point).ClearAxialOnly Motion type: Axial to clearance plane only (no motion to point).-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-