TurnAvoidancePathPointsBuilderPointStatus Enumeration¶
NXOpen.CAM.TurnAvoidancePathPointsBuilder.PointStatus is an alias for NXOpen.CAM.TurnAvoidancePathPointsBuilderPointStatus
-
class
NXOpen.CAM.
TurnAvoidancePathPointsBuilderPointStatus
¶ Bases:
object
the point status options
New in version NX6.0.2.
Enum Members
Enum Member Enum Member Description Inactive Point Status: InactiveActive Point Status: Active-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-