Properties¶
Property | Description |
---|---|
FromPoint | Returns or sets the from point |
FromPointMode | Returns or sets the from point mode |
Tag | Returns the Tag for this object. |
Methods¶
Enumerations¶
TurnAvoidanceFromBuilderFromPointModes Enumeration | The from point mode options |
Property Detail¶
FromPoint¶
-
TurnAvoidanceFromBuilder.
FromPoint
¶ Returns or sets the from point
-------------------------------------
Getter Method
Signature
FromPoint()
Returns: the from point value Return type: NXOpen.Point
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FromPoint(fromPoint)
Parameters: fromPoint ( NXOpen.Point
) – the from point valueNew in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
FromPointMode¶
-
TurnAvoidanceFromBuilder.
FromPointMode
¶ Returns or sets the from point mode
-------------------------------------
Getter Method
Signature
FromPointMode()
Returns: the from point mode value Return type: NXOpen.CAM.TurnAvoidanceFromBuilderFromPointModes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FromPointMode(fromPointMode)
Parameters: fromPointMode ( NXOpen.CAM.TurnAvoidanceFromBuilderFromPointModes
) – the from point mode valueNew in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)