ToolSubtypes Enumeration¶
NXOpen.CAM.Tool.Subtypes is an alias for NXOpen.CAM.ToolSubtypes
-
class
NXOpen.CAM.
ToolSubtypes
¶ Bases:
object
Tool subtypes
Enum Members
Enum Member Enum Member Description Undefined Mill5 Milling tool-5 parametersMill7 Milling tool-7 parametersMill10 Milling tool-10 parametersMillBall Milling tool-Ball millDrillStandard Drilling toolDrillCenterBell CenterdrillDrillCountersink CountersinkDrillSpotFace Spot facing toolDrillSpotDrill Spot drillDrillBore Boring toolDrillReam ReamerDrillCounterbore CounterboreDrillTap TapDrillBurnishing Burnishing toolDrillThreadMill Thread millDrillBackSpotFace Back spot facing toolDrillStep Step drillTurnStandard Turning tool-StandardTurnButton Turning tool-ButtonTurnBoringBar Turning tool-Boring barGrooveStandard Grooving tool-StandardGrooveRing Grooving tool-RingGrooveFullNoseRadius Grooving tool-Full nose radiusGrooveUserDefined Grooving tool-User definedThreadStandard Threading tool-StandardThreadButress Threading tool-ButressThreadAcme Threading tool-ACMEThreadTrapezoidal Threading tool-TrapezoidalGeneric Solid tool genericProbe ProbeMillChamfer Milling chamfer millMillSpherical Milling spherical millDrillCore Core DrillStdLaser Standard Laser toolLaser -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-