ToolPathTiltBuilder Class¶
-
class
NXOpen.CAM.
ToolPathTiltBuilder
¶ Bases:
NXOpen.Builder
Represents a Tool Path Tilt Builder
To create a new instance of this class, use
NXOpen.CAM.CAMSetup.CreateToolPathTiltBuilder
New in version NX7.5.2.
Properties¶
Property | Description |
---|---|
FanDistance | Returns the fan distance |
MaintainTilt | Returns or sets the maintain tilt |
MaxMaintainTiltDistance | Returns the max maintain tilt distance |
MaxTiltAngle | Returns or sets the maximum tilt angle |
MinHolderClearance | Returns the minimum holder clearance |
MinNeckClearance | Returns the minimum neck clearance |
MinSafeClearance | Returns the minimum safeclearance |
MinShankClearance | Returns the minimum shank clearance |
PreferredTiltAngle | Returns or sets the preferred tilt angle |
Tag | Returns the Tag for this object. |
TiltAvoidance | Returns the avoidance builder |
TiltClearance | Returns the clearance builder |
TiltMachine | Returns the machine builder |
TiltTilting | Returns the tilting builder |
ToolAxisChange | Returns or sets the tool axis change |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
FanDistance¶
-
ToolPathTiltBuilder.
FanDistance
¶ Returns the fan distance
-------------------------------------
Getter Method
Signature
FanDistance()
Returns: the fan distance value Return type: NXOpen.CAM.InheritableToolDepBuilder
New in version NX7.5.2.
Deprecated since version NX9.0.0: Use
NXOpen.CAM.ToolPathTiltAvoidance.FanDistance
instead.License requirements: None.
MaintainTilt¶
-
ToolPathTiltBuilder.
MaintainTilt
¶ Returns or sets the maintain tilt
-------------------------------------
Getter Method
Signature
MaintainTilt()
Returns: the value of maintain tilt Return type: bool New in version NX8.5.0.
Deprecated since version NX9.0.0: Use
NXOpen.CAM.ToolPathTiltAvoidance.MaintainTilt
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
MaintainTilt(maintainTilt)
Parameters: maintainTilt (bool) – the value of maintain tilt New in version NX8.5.0.
Deprecated since version NX9.0.0: Use
NXOpen.CAM.ToolPathTiltAvoidance.MaintainTilt
instead.License requirements: None.
MaxMaintainTiltDistance¶
-
ToolPathTiltBuilder.
MaxMaintainTiltDistance
¶ Returns the max maintain tilt distance
-------------------------------------
Getter Method
Signature
MaxMaintainTiltDistance()
Returns: the max maintain tilt distance Return type: NXOpen.CAM.InheritableToolDepBuilder
New in version NX8.5.0.
Deprecated since version NX9.0.0: Use
NXOpen.CAM.ToolPathTiltAvoidance.MaxMaintainTiltDistance
instead.License requirements: None.
MaxTiltAngle¶
-
ToolPathTiltBuilder.
MaxTiltAngle
¶ Returns or sets the maximum tilt angle
-------------------------------------
Getter Method
Signature
MaxTiltAngle()
Returns: the value of maximal tilt angle Return type: float New in version NX7.5.2.
Deprecated since version NX9.0.0: Use
NXOpen.CAM.ToolPathTiltMachine.MaxTiltAngle
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
MaxTiltAngle(maxTiltangle)
Parameters: maxTiltangle (float) – the value of maximal tilt angle New in version NX7.5.2.
Deprecated since version NX9.0.0: Use
NXOpen.CAM.ToolPathTiltMachine.MaxTiltAngle
instead.License requirements: None.
MinHolderClearance¶
-
ToolPathTiltBuilder.
MinHolderClearance
¶ Returns the minimum holder clearance
-------------------------------------
Getter Method
Signature
MinHolderClearance()
Returns: the minimum holder clearance value Return type: NXOpen.CAM.InheritableToolDepBuilder
New in version NX8.0.0.
Deprecated since version NX9.0.0: Use
NXOpen.CAM.ToolPathTiltClearance.MinHolderClearance
instead.License requirements: None.
MinNeckClearance¶
-
ToolPathTiltBuilder.
MinNeckClearance
¶ Returns the minimum neck clearance
-------------------------------------
Getter Method
Signature
MinNeckClearance()
Returns: the minimum neck clearance value Return type: NXOpen.CAM.InheritableToolDepBuilder
New in version NX8.0.0.
Deprecated since version NX9.0.0: Use
NXOpen.CAM.ToolPathTiltClearance.MinNeckClearance
instead.License requirements: None.
MinSafeClearance¶
-
ToolPathTiltBuilder.
MinSafeClearance
¶ Returns the minimum safeclearance
-------------------------------------
Getter Method
Signature
MinSafeClearance()
Returns: the minimum safeclearance value Return type: NXOpen.CAM.InheritableToolDepBuilder
New in version NX7.5.2.
Deprecated since version NX8.0.0: Use
NXOpen.CAM.ToolPathTiltBuilder.MinHolderClearance
instead.License requirements: None.
MinShankClearance¶
-
ToolPathTiltBuilder.
MinShankClearance
¶ Returns the minimum shank clearance
-------------------------------------
Getter Method
Signature
MinShankClearance()
Returns: the minimum shank clearance value Return type: NXOpen.CAM.InheritableToolDepBuilder
New in version NX8.0.0.
Deprecated since version NX9.0.0: Use
NXOpen.CAM.ToolPathTiltClearance.MinShankClearance
instead.License requirements: None.
PreferredTiltAngle¶
-
ToolPathTiltBuilder.
PreferredTiltAngle
¶ Returns or sets the preferred tilt angle
-------------------------------------
Getter Method
Signature
PreferredTiltAngle()
Returns: the value of preferred tilt angle Return type: float New in version NX8.5.0.
Deprecated since version NX9.0.0: Use
NXOpen.CAM.ToolPathTiltAvoidance.PreferredTiltAngle
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
PreferredTiltAngle(preferredAngle)
Parameters: preferredAngle (float) – the value of preferred tilt angle New in version NX8.5.0.
Deprecated since version NX9.0.0: Use
NXOpen.CAM.ToolPathTiltAvoidance.PreferredTiltAngle
instead.License requirements: None.
TiltAvoidance¶
-
ToolPathTiltBuilder.
TiltAvoidance
¶ Returns the avoidance builder
-------------------------------------
Getter Method
Signature
TiltAvoidance()
Returns: the avoidance builder Return type: NXOpen.CAM.ToolPathTiltAvoidance
New in version NX9.0.0.
License requirements: None.
TiltClearance¶
-
ToolPathTiltBuilder.
TiltClearance
¶ Returns the clearance builder
-------------------------------------
Getter Method
Signature
TiltClearance()
Returns: the clearance builder Return type: NXOpen.CAM.ToolPathTiltClearance
New in version NX9.0.0.
License requirements: None.
TiltMachine¶
-
ToolPathTiltBuilder.
TiltMachine
¶ Returns the machine builder
-------------------------------------
Getter Method
Signature
TiltMachine()
Returns: the machine builder Return type: NXOpen.CAM.ToolPathTiltMachine
New in version NX9.0.0.
License requirements: None.
TiltTilting¶
-
ToolPathTiltBuilder.
TiltTilting
¶ Returns the tilting builder
-------------------------------------
Getter Method
Signature
TiltTilting()
Returns: the tilting builder Return type: NXOpen.CAM.ToolPathTiltTilting
New in version NX9.0.0.
License requirements: None.
ToolAxisChange¶
-
ToolPathTiltBuilder.
ToolAxisChange
¶ Returns or sets the tool axis change
-------------------------------------
Getter Method
Signature
ToolAxisChange()
Returns: the value of toolaxis change Return type: float New in version NX7.5.2.
Deprecated since version NX9.0.0: Use
NXOpen.CAM.ToolPathTiltMachine.MaxToolAxisChange
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
ToolAxisChange(toolaxisChange)
Parameters: toolaxisChange (float) – the value of maximum tool axis change New in version NX7.5.2.
Deprecated since version NX9.0.0: Use
NXOpen.CAM.ToolPathTiltMachine.MaxToolAxisChange
instead.License requirements: None.
Method Detail¶
Validate¶
-
ToolPathTiltBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.