ToolPathTiltAvoidanceMethodType Enumeration¶
NXOpen.CAM.ToolPathTiltAvoidance.MethodType is an alias for NXOpen.CAM.ToolPathTiltAvoidanceMethodType
-
class
NXOpen.CAM.
ToolPathTiltAvoidanceMethodType
¶ Bases:
object
the collision avoidance method type
Enum Members
Enum Member Enum Member Description Tilt Avoidance method: tiltRetract Avoidance method: retract-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-