ToolPathSplitParametersBuilderTransferTypes Enumeration¶
NXOpen.CAM.ToolPathSplitParametersBuilder.TransferTypes is an alias for NXOpen.CAM.ToolPathSplitParametersBuilderTransferTypes
-
class
NXOpen.CAM.
ToolPathSplitParametersBuilderTransferTypes
¶ Bases:
object
Transfer type options
Enum Members
Enum Member Enum Member Description Direct direct transfer typeClearance clearance transfer typeLowestSafeZ lowest safe z transfer typeSmooth smooth transfer typePlane local plane transfer type-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-