ToolPathDisplay Class¶
-
class
NXOpen.CAM.
ToolPathDisplay
¶ Bases:
object
Represents a class that is used for NX testing.
This class should not be made available to customers To obtain an instance of this class, refer to
NXOpen.DebugSession
New in version NX9.0.2.
Methods¶
Method | Description |
---|---|
ButtonDown | Debug Trace user button presses. |
HideToolPath | Hide tool path |
SetColorBy | Set the option for coloring the tool path motions. |
ShowCutting | Displays the cutting moves in a milling tool path. |
ShowEndpoints | Displays a symbol at the end of each motion. |
ShowNoncutting | Displays the non cutting moves in a milling tool path. |
ShowToolCenter | Displays the tool path at the tool center instead of the tool tip for a ball mill. |
ShowToolPath | Show tool path |
Table | Debug Table of tool path display motions |
Timer | Debug Measure display time |
Trace | Debug Trace display functions |
Enumerations¶
ToolPathDisplayColorBy Enumeration | Choices for coloring the tool path motions |
Method Detail¶
ButtonDown¶
-
ToolPathDisplay.
ButtonDown
¶ Debug Trace user button presses.
Signature
ButtonDown(isOn)
Parameters: isOn (bool) – New in version NX9.0.2.
License requirements: None.
HideToolPath¶
-
ToolPathDisplay.
HideToolPath
¶ Hide tool path
Signature
HideToolPath(opr)
Parameters: opr ( NXOpen.CAM.CAMObject
) –New in version NX9.0.2.
License requirements: None.
SetColorBy¶
-
ToolPathDisplay.
SetColorBy
¶ Set the option for coloring the tool path motions.
Signature
SetColorBy(colorBy)
Parameters: colorBy ( NXOpen.CAM.ToolPathDisplayColorBy
) –New in version NX9.0.2.
License requirements: None.
ShowCutting¶
-
ToolPathDisplay.
ShowCutting
¶ Displays the cutting moves in a milling tool path.
Signature
ShowCutting(isOn)
Parameters: isOn (bool) – New in version NX9.0.2.
License requirements: None.
ShowEndpoints¶
-
ToolPathDisplay.
ShowEndpoints
¶ Displays a symbol at the end of each motion.
Signature
ShowEndpoints(isOn)
Parameters: isOn (bool) – New in version NX9.0.2.
License requirements: None.
ShowNoncutting¶
-
ToolPathDisplay.
ShowNoncutting
¶ Displays the non cutting moves in a milling tool path.
Signature
ShowNoncutting(isOn)
Parameters: isOn (bool) – New in version NX9.0.2.
License requirements: None.
ShowToolCenter¶
-
ToolPathDisplay.
ShowToolCenter
¶ Displays the tool path at the tool center instead of the tool tip for a ball mill.
Signature
ShowToolCenter(isOn)
Parameters: isOn (bool) – New in version NX9.0.2.
License requirements: None.
ShowToolPath¶
-
ToolPathDisplay.
ShowToolPath
¶ Show tool path
Signature
ShowToolPath(opr)
Parameters: opr ( NXOpen.CAM.CAMObject
) –New in version NX9.0.2.
License requirements: None.
Table¶
-
ToolPathDisplay.
Table
¶ Debug Table of tool path display motions
Signature
Table(isOn)
Parameters: isOn (bool) – New in version NX9.0.2.
License requirements: None.