ToolAxisVariableTypes Enumeration¶
NXOpen.CAM.ToolAxisVariable.Types is an alias for NXOpen.CAM.ToolAxisVariableTypes
-
class
NXOpen.CAM.
ToolAxisVariableTypes
¶ Bases:
object
Available types for Tool Axis Variable
Enum Members
Enum Member Enum Member Description AwayFromPoint Away from PointTowardPoint Toward PointAwayFromLine Away from LineTowardLine Toward LineRelativeToVector Relative to VectorNormalToPart Normal to PartRelativeToPart Relative to PartFourAxisNormalToPart 4-Axis Normal to PartFourAxisRelativeToPart 4-Axis Relative to PartDualFourAxisOnPart Dual 4-Axis on PartInterpolateVector Interpolate VectorInterpolateAngleToPart Interpolate Angle to PartInterpolateAngleToDrive Interpolate Angle to DriveOptimizedToDrive Optimized to DriveNormalToDrive Normal to DriveSwarfDrive Swarf DriveRelativeToDrive Relative to DriveFourAxisNormalToDrive 4-Axis Normal to DriveFourAxisRelativeToDrive 4-Axis Relative to DriveDualFourAxisOnDrive Dual 4-Axis on DriveSameAsDrivePath Same as drive pathUserDefined User DefinedAutomatic Original VAP tool axisAlignToEdges Align to almost straight edgesSwarfBaseUV Align to U or V parameter lineFourAxisAroundRotaryAxis 4-Axis Around Rotary Axis-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-