ToolAxisFixed Class¶
-
class
NXOpen.CAM.
ToolAxisFixed
¶ Bases:
NXOpen.CAM.ToolAxisBase
Represents a Tool Axis Fixed Builder
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
Point | Returns or sets the Point |
Tag | Returns the Tag for this object. |
ToolAxisType | Returns or sets the tool axis types |
Vector | Returns or sets the Vector |
Methods¶
Enumerations¶
ToolAxisFixedTypes Enumeration | Available types for Tool Axis Fixed |
Property Detail¶
ToolAxisType¶
-
ToolAxisFixed.
ToolAxisType
¶ Returns or sets the tool axis types
-------------------------------------
Getter Method
Signature
ToolAxisType()
Returns: the tool axis type Return type: NXOpen.CAM.ToolAxisFixedTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ToolAxisType(toolAxis)
Parameters: toolAxis ( NXOpen.CAM.ToolAxisFixedTypes
) – the tool axis typeNew in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)