SurfaceContourBuilderDriveMethodTypes Enumeration¶
NXOpen.CAM.SurfaceContourBuilder.DriveMethodTypes is an alias for NXOpen.CAM.SurfaceContourBuilderDriveMethodTypes
-
class
NXOpen.CAM.
SurfaceContourBuilderDriveMethodTypes
¶ Bases:
object
Available types for Drive Method
Enum Members
Enum Member Enum Member Description Undef UndefinedCurve Curve/PointSpiral SpiralBoundary BoundaryAreaMilling Area MillingSurfaceArea Surface AreaInterpolatedToolPath Interpolated tool pathToolPath Tool PathRadialCut Radial CutContourProfile Contour ProfileFlowCut Flow CutText TextUserDefined User FunctionBladeRough Blade RoughBladeFinish Blade FinishHubFinish Hub FinishBlendFinish Blend FinishEdgeFinish Edge FinishRotaryFloorFinish Rotary Floor FinishTotal Total-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-