Splitter Class¶
-
class
NXOpen.CAM.
Splitter
¶ Bases:
NXOpen.TaggedObject
Represents a Splitter Builder
To create a new instance of this class, use
NXOpen.CAM.MultiBladeSplittersGeometry.CreateSplitter
New in version NX7.0.0.
Properties¶
Property | Description |
---|---|
CountOfFaces | Returns or sets the item count of the list |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
GetBlendFaces | Get the blend faces @return the blend faces |
GetWallFaces | Get the wall faces @return the wall faces |
RemoveBlendFaces | Remove the blend faces |
RemoveWallFaces | Remove the wall faces |
SetBlendFaces | Set the blend faces |
SetWallFaces | Set the wall faces |
Property Detail¶
CountOfFaces¶
-
Splitter.
CountOfFaces
¶ Returns or sets the item count of the list
-------------------------------------
Getter Method
Signature
CountOfFaces()
Returns: the count of the list Return type: int New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CountOfFaces(count)
Parameters: count (int) – the count of the list New in version NX7.0.0.
License requirements: cam_base (“CAM BASE”)
Method Detail¶
GetBlendFaces¶
-
Splitter.
GetBlendFaces
¶ Get the blend faces
Signature
GetBlendFaces()
Returns: the blend faces Return type: list of NXOpen.NXObject
New in version NX7.0.0.
License requirements: None.
GetWallFaces¶
-
Splitter.
GetWallFaces
¶ Get the wall faces
Signature
GetWallFaces()
Returns: the wall faces Return type: list of NXOpen.NXObject
New in version NX7.0.0.
License requirements: None.
RemoveBlendFaces¶
-
Splitter.
RemoveBlendFaces
¶ Remove the blend faces
Signature
RemoveBlendFaces(faces)
Parameters: faces (list of NXOpen.NXObject
) – the removed blend facesNew in version NX7.0.0.
License requirements: cam_base (“CAM BASE”)
RemoveWallFaces¶
-
Splitter.
RemoveWallFaces
¶ Remove the wall faces
Signature
RemoveWallFaces(faces)
Parameters: faces (list of NXOpen.NXObject
) – the removed wall facesNew in version NX7.0.0.
License requirements: cam_base (“CAM BASE”)
SetBlendFaces¶
-
Splitter.
SetBlendFaces
¶ Set the blend faces
Signature
SetBlendFaces(blendFaces)
Parameters: blendFaces (list of NXOpen.NXObject
) – the blend facesNew in version NX7.0.0.
License requirements: cam_base (“CAM BASE”)
SetWallFaces¶
-
Splitter.
SetWallFaces
¶ Set the wall faces
Signature
SetWallFaces(wallFaces)
Parameters: wallFaces (list of NXOpen.NXObject
) – the wall facesNew in version NX7.0.0.
License requirements: cam_base (“CAM BASE”)