SmallAreaAvoidance Class¶
-
class
NXOpen.CAM.
SmallAreaAvoidance
¶ Bases:
NXOpen.TaggedObject
Represents a SmallArea Builder
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
AreaSize | Returns the area size |
SmallAreaStatus | Returns or sets the small area status |
Tag | Returns the Tag for this object. |
Methods¶
Enumerations¶
SmallAreaAvoidanceStatusTypes Enumeration | available types for Small Area Status |
Property Detail¶
AreaSize¶
-
SmallAreaAvoidance.
AreaSize
¶ Returns the area size
-------------------------------------
Getter Method
Signature
AreaSize()
Returns: the area size builder Return type: NXOpen.CAM.InheritableToolDepBuilder
New in version NX6.0.0.
License requirements: None.
SmallAreaStatus¶
-
SmallAreaAvoidance.
SmallAreaStatus
¶ Returns or sets the small area status
-------------------------------------
Getter Method
Signature
SmallAreaStatus()
Returns: Return type: NXOpen.CAM.SmallAreaAvoidanceStatusTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SmallAreaStatus(newValue)
Parameters: newValue ( NXOpen.CAM.SmallAreaAvoidanceStatusTypes
) –New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)