RoundPointBuilder Class¶
-
class
NXOpen.CAM.
RoundPointBuilder
¶ Bases:
NXOpen.TaggedObject
Represents the round Point Builder
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
Decimals | Returns or sets the decimal places |
Rounding | Returns or sets the rounding status |
Tag | Returns the Tag for this object. |
Methods¶
Enumerations¶
RoundPointBuilderOutput Enumeration | the decimal places |
Property Detail¶
Decimals¶
-
RoundPointBuilder.
Decimals
¶ Returns or sets the decimal places
-------------------------------------
Getter Method
Signature
Decimals()
Returns: Return type: NXOpen.CAM.RoundPointBuilderOutput
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Decimals(decimals)
Parameters: decimals ( NXOpen.CAM.RoundPointBuilderOutput
) –New in version NX5.0.0.
License requirements: None.
Rounding¶
-
RoundPointBuilder.
Rounding
¶ Returns or sets the rounding status
-------------------------------------
Getter Method
Signature
Rounding()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Rounding(rounding)
Parameters: rounding (bool) – New in version NX5.0.0.
License requirements: None.