RampingModeTypes Enumeration¶
NXOpen.CAM.RampingMode.Types is an alias for NXOpen.CAM.RampingModeTypes
-
class
NXOpen.CAM.
RampingModeTypes
¶ Bases:
object
the ramping mode options
New in version NX6.0.0.
Enum Members
Enum Member Enum Member Description RampOutOnEveryOtherPass Ramping mode: Ramp Out on every other PassRampInOnEveryOtherPass Ramping mode: Ramp In on every other PassRampOutFirst Ramping mode: Ramp Out firstRampInFirst Ramping mode: Ramp In first-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-