ProjVecCiBuilderDpmProjTypes Enumeration¶
NXOpen.CAM.ProjVecCiBuilder.DpmProjTypes is an alias for NXOpen.CAM.ProjVecCiBuilderDpmProjTypes
-
class
NXOpen.CAM.
ProjVecCiBuilderDpmProjTypes
¶ Bases:
object
Available types for Project Vector
Enum Members
Enum Member Enum Member Description ProjVecFixed Specify VectorProjVecToolAxis Tool AxisProjVecFromPoint way from PointProjVecToPoint Toward PointProjVecFromLine Away from LineProjVecToLine Toward LineProjVecNormToDrive Normal to DriveProjVecToDrive Toward DriveProjVecRuling Swarf RulingProjVecUserDefined User FunctionProjVecToolAxisUp Tool Axis upProjVecTotal Total-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-