ProbeInspectSurfacePointMoveBuilderToolAxis Enumeration¶
NXOpen.CAM.ProbeInspectSurfacePointMoveBuilder.ToolAxis is an alias for NXOpen.CAM.ProbeInspectSurfacePointMoveBuilderToolAxis
-
class
NXOpen.CAM.
ProbeInspectSurfacePointMoveBuilderToolAxis
¶ Bases:
object
the probing tool axis type
Enum Members
Enum Member Enum Member Description None Use the Previous Tool AxisNormal Inferred using surface normalAutomatic Tool Axis aligned with closest machine axis-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-