ProbeClearanceMoveBuilder Class¶
-
class
NXOpen.CAM.
ProbeClearanceMoveBuilder
¶ Bases:
NXOpen.CAM.MoveBuilder
Represents the Probe Clearance Move Builder
To create a new instance of this class, use
NXOpen.CAM.MoveCollection.CreateProbeClearanceMoveBuilder
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
ClearanceBuilder | Returns the NCM clearance builder |
FeedRate | Returns or sets the feed rate |
FeedType | Returns or sets the feed type |
FeedUnit | Returns or sets the feed unit |
MotionType | Returns or sets the motion type |
NumberOfUserParameters | Returns the number of user parameters |
ProtectedMove | Returns or sets the protected move status |
SubopLabel | Returns or sets the subop label |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
GetUserParameter | Returns the custom parameter with the given name. |
SetParent | Set parent |
SetSibling | Set sibling |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
ClearanceBuilder¶
-
ProbeClearanceMoveBuilder.
ClearanceBuilder
¶ Returns the NCM clearance builder
-------------------------------------
Getter Method
Signature
ClearanceBuilder()
Returns: Clearance Builder Return type: NXOpen.CAM.NcmClearanceBuilder
New in version NX5.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
ProbeClearanceMoveBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.