NcmWedmBuilderCutcomOffTypes Enumeration¶
NXOpen.CAM.NcmWedmBuilder.CutcomOffTypes is an alias for NXOpen.CAM.NcmWedmBuilderCutcomOffTypes
-
class
NXOpen.CAM.
NcmWedmBuilderCutcomOffTypes
¶ Bases:
object
the types available for cutcom off
New in version NX7.5.0.
Enum Members
Enum Member Enum Member Description None no cutcom offBeforeLeadOut cutcom off before lead outAfterLeadOut cutcom off after lead outBeforeThreadPoint cutcom off before thread point-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-