NcmTurnThreadBuilderLocalReturnTypes Enumeration¶
NXOpen.CAM.NcmTurnThreadBuilder.LocalReturnTypes is an alias for NXOpen.CAM.NcmTurnThreadBuilderLocalReturnTypes
-
class
NXOpen.CAM.
NcmTurnThreadBuilderLocalReturnTypes
¶ Bases:
object
The Cut regions type options
New in version NX6.0.0.
Enum Members
Enum Member Enum Member Description None NoneDirect DirectRadialAxial Radial-AxialAxialRadial Axial-RadialClearRadialDirect Clear Radial-DirectClearAxialDirect Clear Axial-DirectClearRadial Clear RadialClearAxial Clear AxialRadialClearAxialDirect Radial-Clear Axial-DirectRadialAxialRadial Radial-Axial-RadialRadialClearAxial Radial-Clear AxialClearRadialClearAxialDirect Clear Radial-Clear Axial-DirectClearRadialAxialRadial Clear Radial-Axial-RadialClearRadialClearAxial Clear Radial-Clear Axial-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-