NcmTransferBuilderAppDepMethodTypes Enumeration¶
NXOpen.CAM.NcmTransferBuilder.AppDepMethodTypes is an alias for NXOpen.CAM.NcmTransferBuilderAppDepMethodTypes
-
class
NXOpen.CAM.
NcmTransferBuilderAppDepMethodTypes
¶ Bases:
object
Available methods for approach and departure
Enum Members
Enum Member Enum Member Description Same use setting from transfer between regionsNone noneAlongToolAxis along tool axisAlongVector along vectorToolAxisClearance along tool axis from/to clearanceShortestDistanceClearance shortest distance from/to clearanceVectorClearance along vector from/to clearanceTangentClearance tangent from/to clearanceAutomatic automatic-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-