NcmScEngRetBuilderEngRetTypes Enumeration¶
NXOpen.CAM.NcmScEngRetBuilder.EngRetTypes is an alias for NXOpen.CAM.NcmScEngRetBuilderEngRetTypes
-
class
NXOpen.CAM.
NcmScEngRetBuilderEngRetTypes
¶ Bases:
object
Available types for engage/retract in surface contouring
Enum Members
Enum Member Enum Member Description SameAsDefault Same as DefaultSameAsEngage Same as Engage (only for retract)Linear LinearLinearAlongVector Linear - Along VectorLinearNormalToPart Linear - Normal to PartArcParallelToToolAxis Arc - Parallel to Tool AxisArcNormalToToolAxis Arc - Normal to Tool AxisArcTangentToApproach Arc - Tangent to ApproachArcNormalToPart Arc - Normal to PartHelicalClw Helical ClockwiseHelicalCclw Helical Counter ClockwisePlungeLift Plunge Engage/Lift RetractNone NonePoints to-from pointSmooth Smooth connections-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-