NcmPlanarEngRetBuilderMeasureHeightFrom Enumeration¶
NXOpen.CAM.NcmPlanarEngRetBuilder.MeasureHeightFrom is an alias for NXOpen.CAM.NcmPlanarEngRetBuilderMeasureHeightFrom
-
class
NXOpen.CAM.
NcmPlanarEngRetBuilderMeasureHeightFrom
¶ Bases:
object
Available types for the Height From which engage helical/ramp/plunge is measured in Planar Milling
Enum Members
Enum Member Enum Member Description CurrentLevel Measure from current levelPreviousLevel Measure from previous levelPlane Measure from user-defined plane-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-