NcmPlanarBuilderPredrillPointsOutputOptions Enumeration¶
NXOpen.CAM.NcmPlanarBuilder.PredrillPointsOutputOptions is an alias for NXOpen.CAM.NcmPlanarBuilderPredrillPointsOutputOptions
-
class
NXOpen.CAM.
NcmPlanarBuilderPredrillPointsOutputOptions
¶ Bases:
object
Available options for output of pre-drill points in planar milling
Enum Members
Enum Member Enum Member Description None No Pre-Drill pointsAllRegions Pre-Drill Points for all regionsBottomRegions Pre-Drill Points for bottom regions only-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-