NcmHoleDrilling Class¶
-
class
NXOpen.CAM.
NcmHoleDrilling
¶ Bases:
NXOpen.CAM.NcmHoleMachining
Represents a
NXOpen.CAM.NcmHoleDrilling
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
CollisionCheck | Returns or sets the collision check activation |
CutcomMinimumAngle | Returns or sets the cutter compensation minimum angle |
CutcomMinimumMove | Returns the cutter compensation minimum move builder (inheritable tool dep) |
CutcomOutputContactPoint | Returns or sets the cutter compensation output contact point status |
CutcomOutputPlane | Returns or sets the cutter compensation output plane status |
CutcomType | Returns or sets the cutter compensation type |
DefaultRegionStartType | Returns or sets the region start type |
Engage | Returns the engage settings |
FinalRetract | Returns the final retract settings |
FinalSafeDistance | Returns the final safe distance builder (inheritable tool dep) |
FinalType | Returns or sets the final type |
InitialEngage | Returns the initial engage settings |
InitialSafeDistance | Returns the initial safe distance builder (inheritable tool dep) |
InitialType | Returns or sets the initial type |
NumberOfThreads | Returns or sets the number of threads |
OverlapAngle | Returns or sets the overlap angle |
OverlapDistance | Returns or sets the overlap distance |
OverlapType | Returns or sets the region start type |
RegionStartAngle | Returns or sets the region start angle |
Retract | Returns the retract settings |
StartFromCenter | Returns or sets the start from center |
StartPointsEffectDistBuilder | Returns the region start points effective distance builder (inheritable tool dep) |
StartPointsUseEffectDist | Returns or sets the start points use effective distance |
SuppressCutcom | Returns or sets the suppress cutter compensation |
Tag | Returns the Tag for this object. |
TrackingData | Returns or sets the tracking data (tracking point type) |
TransferAvoidanceFrom | Returns the from point builder |
TransferAvoidanceGohome | Returns the gohome point builder |
TransferAvoidanceReturn | Returns the return point builder |
TransferAvoidanceStart | Returns the start point builder |
TransferBetweenRegions | Returns the transfer between regions |
TransferClearance | Returns the clearance setting |
TransferInitialFinal | Returns the transfer settings for initial and final |
Methods¶
Method | Description |
---|---|
GetRegionStartPoints | Returns region start points |
SetRegionStartPoints | Sets region start points |