MultiRamp Class¶
-
class
NXOpen.CAM.
MultiRamp
¶ Bases:
NXOpen.TaggedObject
Represents a
NXOpen.CAM.MultiRamp
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
MaxRampLength | Returns the maximum ramp length |
Pattern | Returns or sets the multi ramp pattern |
Tag | Returns the Tag for this object. |
Methods¶
Enumerations¶
MultiRampTypes Enumeration | the multi ramp pattern types |
Property Detail¶
MaxRampLength¶
-
MultiRamp.
MaxRampLength
¶ Returns the maximum ramp length
-------------------------------------
Getter Method
Signature
MaxRampLength()
Returns: the maximum ramp length Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX6.0.0.
License requirements: None.
Pattern¶
-
MultiRamp.
Pattern
¶ Returns or sets the multi ramp pattern
-------------------------------------
Getter Method
Signature
Pattern()
Returns: the multi ramp pattern Return type: NXOpen.CAM.MultiRampTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Pattern(multiRampPattern)
Parameters: multiRampPattern ( NXOpen.CAM.MultiRampTypes
) – the multi ramp patternNew in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)