MinCutVolume Class¶
-
class
NXOpen.CAM.
MinCutVolume
¶ Bases:
NXOpen.TaggedObject
Represents a
NXOpen.CAM.MinCutVolume
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
SuppressBasedOnVolume | Returns or sets the suppress path if less than minimum toggle |
Tag | Returns the Tag for this object. |
VolumeThreshold | Returns or sets the minimum volume percentage |
Methods¶
Property Detail¶
SuppressBasedOnVolume¶
-
MinCutVolume.
SuppressBasedOnVolume
¶ Returns or sets the suppress path if less than minimum toggle
-------------------------------------
Getter Method
Signature
SuppressBasedOnVolume()
Returns: the minimum cut volume usage Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SuppressBasedOnVolume(propValue)
Parameters: propValue (bool) – the minimum cut volume usage New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
VolumeThreshold¶
-
MinCutVolume.
VolumeThreshold
¶ Returns or sets the minimum volume percentage
-------------------------------------
Getter Method
Signature
VolumeThreshold()
Returns: the cut volume minimum percentage Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VolumeThreshold(propValue)
Parameters: propValue (float) – the cut volume minimum percentage New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)