MachinePocketGroupBuilderRegisterType Enumeration¶
NXOpen.CAM.MachinePocketGroupBuilder.RegisterType is an alias for NXOpen.CAM.MachinePocketGroupBuilderRegisterType
-
class
NXOpen.CAM.
MachinePocketGroupBuilderRegisterType
¶ Bases:
object
the register type
Deprecated since version NX8.5.0: This
NXOpen.CAM.MachinePocketGroupBuilderRegisterType
is no longer supported.Enum Members
Enum Member Enum Member Description SameAsPocketId use same as pocket idSpecify use specify-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-