LaserTeachMode Class¶
-
class
NXOpen.CAM.
LaserTeachMode
¶ Bases:
NXOpen.CAM.OperationBuilder
Represents a Laser TeachMode
To create a new instance of this class, use
NXOpen.CAM.OperationCollection.CreateLaserTeachMode
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
ChannelName | Returns or sets the channel’s name |
CycleEvent | Returns the cycle event |
CycleTable | Returns the cycle |
Description | Returns or sets the description |
EndOfPath | Returns the end event builder |
EndUdeSet | Returns the end ude set |
Feeds | Returns the feeds and speeds |
Geometry | Returns the geometry builder |
GougeChecking | Returns or sets the gouge checking flag |
HoleAxisType | Returns or sets the Hole Axis Type |
HoleDepth | Returns the max depth distance builder |
HoleDepthType | Returns or sets the Hole Depth Type |
LayoutAndLayer | Returns the Layer and Layout |
MotionOutputBuilder | Returns the motion output builder |
NcmEngage | Returns the ncm engage |
NcmRetract | Returns the ncm retract |
Notes | Returns the notes builder |
OptimizationBasedOn | Returns or sets the optimization based on in operation |
OptimizationDistanceMethod | Returns or sets the optimization distance method in operation |
OptimizationLevel | Returns or sets the optimization level in operation |
OptimizationMethod | Returns or sets the optim method |
OverlapDistance | Returns the Overlap Distance |
PathDisplayOptions | Returns the path display options builder |
RetractDistance | Returns the Retract Distance builder (inheritable double) |
RetractDistanceOnToolAxisChange | Returns the Retract Distance on Tool Axis Change builder (inheritable double) |
SafeClearance | Returns the safe clearance builder |
SelectToolFlag | Returns or sets the user selected tool |
StartOfPath | Returns the start event builder |
StartUdeSet | Returns the start ude set |
Tag | Returns the Tag for this object. |
ToolChangeSetting | Returns the tool change builder |
ToolPathSplitParametersBuilder | Returns the tool path split Parameters |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetHoleAxisValues | Get the Hole Axis values @return the Hole Axis values |
GetObject | Returns the object currently being edited by this builder. |
SetHoleAxisValues | Set the Hole Axis values |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Feeds¶
-
LaserTeachMode.
Feeds
¶ Returns the feeds and speeds
-------------------------------------
Getter Method
Signature
Feeds()
Returns: Return type: NXOpen.CAM.FeedsBuilder
New in version NX9.0.0.
License requirements: None.
NcmEngage¶
-
LaserTeachMode.
NcmEngage
¶ Returns the ncm engage
-------------------------------------
Getter Method
Signature
NcmEngage()
Returns: Return type: NXOpen.CAM.NcmLaserEngage
New in version NX9.0.0.
License requirements: None.
NcmRetract¶
-
LaserTeachMode.
NcmRetract
¶ Returns the ncm retract
-------------------------------------
Getter Method
Signature
NcmRetract()
Returns: Return type: NXOpen.CAM.NcmLaserRetract
New in version NX9.0.0.
License requirements: None.
OverlapDistance¶
-
LaserTeachMode.
OverlapDistance
¶ Returns the Overlap Distance
-------------------------------------
Getter Method
Signature
OverlapDistance()
Returns: Return type: NXOpen.CAM.InheritableToolDepBuilder
New in version NX9.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
LaserTeachMode.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.