LaserMethod Class¶
-
class
NXOpen.CAM.
LaserMethod
¶ Bases:
NXOpen.CAM.MethodBuilder
Represents a Laser Method
To create a new instance of this class, use
NXOpen.CAM.NCGroupCollection.CreateLaserMethod
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
CutGasPressure | Returns the Cut Gas Pressure |
CutGasType | Returns the Cut Gas Type |
CutLaserDelay | Returns the Cut Laser Delay |
CutLaserFrequency | Returns the Cut Laser Frequency |
CutLaserPower | Returns the Cut Laser Power |
CutParameters | Returns the cut parameter object |
CycleEvent | Returns the cycle event |
CycleTable | Returns the cycle |
Description | Returns or sets the description |
EndUdeSet | Returns the end ude set |
Feeds | Returns the feeds |
OptimizationMethod | Returns or sets the optim method |
PaintDisplay | Returns the sub builder for paint display |
PathDisplay | Returns the sub builder for path display |
PathDisplayColors | Returns the sub builder for path display colors |
PierceGasPressure | Returns the Pierce Gas Pressure |
PierceGasType | Returns the Pierce Gas Type |
PierceLaserDelay | Returns the Pierce Laser Delay |
PierceLaserFrequency | Returns the Pierce Laser Frequency |
PierceLaserPower | Returns the Pierce Laser Power |
SilhouDisplay | Returns the sub builder for silhou display |
StartUdeSet | Returns the start ude set |
Tag | Returns the Tag for this object. |
ToolDisplay | Returns the sub builder for tool display |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetCutMethod | Get cut method @return |
GetObject | Returns the object currently being edited by this builder. |
SetCutMethod | Set cut method |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
CutGasPressure¶
-
LaserMethod.
CutGasPressure
¶ Returns the Cut Gas Pressure
-------------------------------------
Getter Method
Signature
CutGasPressure()
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX9.0.0.
License requirements: None.
CutGasType¶
-
LaserMethod.
CutGasType
¶ Returns the Cut Gas Type
-------------------------------------
Getter Method
Signature
CutGasType()
Returns: Return type: NXOpen.CAM.InheritableIntBuilder
New in version NX9.0.0.
License requirements: None.
CutLaserDelay¶
-
LaserMethod.
CutLaserDelay
¶ Returns the Cut Laser Delay
-------------------------------------
Getter Method
Signature
CutLaserDelay()
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX9.0.0.
License requirements: None.
CutLaserFrequency¶
-
LaserMethod.
CutLaserFrequency
¶ Returns the Cut Laser Frequency
-------------------------------------
Getter Method
Signature
CutLaserFrequency()
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX9.0.0.
License requirements: None.
CutLaserPower¶
-
LaserMethod.
CutLaserPower
¶ Returns the Cut Laser Power
-------------------------------------
Getter Method
Signature
CutLaserPower()
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX9.0.0.
License requirements: None.
Feeds¶
-
LaserMethod.
Feeds
¶ Returns the feeds
-------------------------------------
Getter Method
Signature
Feeds()
Returns: the feeds builder Return type: NXOpen.CAM.FeedsBuilder
New in version NX9.0.0.
License requirements: None.
PierceGasPressure¶
-
LaserMethod.
PierceGasPressure
¶ Returns the Pierce Gas Pressure
-------------------------------------
Getter Method
Signature
PierceGasPressure()
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX9.0.0.
License requirements: None.
PierceGasType¶
-
LaserMethod.
PierceGasType
¶ Returns the Pierce Gas Type
-------------------------------------
Getter Method
Signature
PierceGasType()
Returns: Return type: NXOpen.CAM.InheritableIntBuilder
New in version NX9.0.0.
License requirements: None.
PierceLaserDelay¶
-
LaserMethod.
PierceLaserDelay
¶ Returns the Pierce Laser Delay
-------------------------------------
Getter Method
Signature
PierceLaserDelay()
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX9.0.0.
License requirements: None.
PierceLaserFrequency¶
-
LaserMethod.
PierceLaserFrequency
¶ Returns the Pierce Laser Frequency
-------------------------------------
Getter Method
Signature
PierceLaserFrequency()
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX9.0.0.
License requirements: None.
PierceLaserPower¶
-
LaserMethod.
PierceLaserPower
¶ Returns the Pierce Laser Power
-------------------------------------
Getter Method
Signature
PierceLaserPower()
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX9.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
LaserMethod.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.