InspectionPlaneFeatureBuilder Class¶
-
class
NXOpen.CAM.
InspectionPlaneFeatureBuilder
¶ Bases:
NXOpen.CAM.OperationBuilder
Represents a CMM Inspection Plane Feature builder
To create a new instance of this class, use
NXOpen.CAM.InspectionOperationCollection.CreateInspectionPlaneFeatureBuilder
New in version NX7.0.0.
Properties¶
Property | Description |
---|---|
BasePointX | Returns or sets the base point or plane center X coordinate |
BasePointY | Returns or sets the base point or plane center Y coordinate |
BasePointZ | Returns or sets the base point or plane center Z coordinate |
ChannelName | Returns or sets the channel’s name |
CsysReferenceType | Returns or sets the csys reference type |
CycleEvent | Returns the cycle event |
CycleTable | Returns the cycle |
Description | Returns or sets the description |
EndOfPath | Returns the end event builder |
EndUdeSet | Returns the end ude set |
ExtentType | Returns or sets the extent type |
Geometry | Returns the geometry builder |
GougeChecking | Returns or sets the gouge checking flag |
HoleAxisType | Returns or sets the Hole Axis Type |
HoleDepth | Returns the max depth distance builder |
HoleDepthType | Returns or sets the Hole Depth Type |
LayoutAndLayer | Returns the Layer and Layout |
MotionOutputBuilder | Returns the motion output builder |
Name | Returns or sets the plane inspection feature name |
NormalVector | Returns or sets the normal vector |
NormalVectorI | Returns or sets the normal vector I component |
NormalVectorJ | Returns or sets the normal vector J component |
NormalVectorK | Returns or sets the normal vector K component |
Notes | Returns the notes builder |
OptimizationBasedOn | Returns or sets the optimization based on in operation |
OptimizationDistanceMethod | Returns or sets the optimization distance method in operation |
OptimizationLevel | Returns or sets the optimization level in operation |
OptimizationMethod | Returns or sets the optim method |
PathDisplayOptions | Returns the path display options builder |
RetractDistance | Returns the Retract Distance builder (inheritable double) |
RetractDistanceOnToolAxisChange | Returns the Retract Distance on Tool Axis Change builder (inheritable double) |
ReverseFaceNormal | Returns or sets the reverse face normal flag |
SafeClearance | Returns the safe clearance builder |
SelectToolFlag | Returns or sets the user selected tool |
SelectedPlane | Returns the selected plane |
StartOfPath | Returns the start event builder |
StartUdeSet | Returns the start ude set |
Tag | Returns the Tag for this object. |
ToolChangeSetting | Returns the tool change builder |
ToolPathSplitParametersBuilder | Returns the tool path split Parameters |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
FlipNormal | Flips the plane inspection feature normal vector |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetHoleAxisValues | Get the Hole Axis values @return the Hole Axis values |
GetObject | Returns the object currently being edited by this builder. |
SetHoleAxisValues | Set the Hole Axis values |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UpdateNormalVector | Updates plane inspection feature normal vector based on selected vector |
UpdateParams | Updates plane inspection feature characteristic parameters based on selected geometry |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
BasePointX¶
-
InspectionPlaneFeatureBuilder.
BasePointX
¶ Returns or sets the base point or plane center X coordinate
-------------------------------------
Getter Method
Signature
BasePointX()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BasePointX(basePointX)
Parameters: basePointX (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
BasePointY¶
-
InspectionPlaneFeatureBuilder.
BasePointY
¶ Returns or sets the base point or plane center Y coordinate
-------------------------------------
Getter Method
Signature
BasePointY()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BasePointY(basePointY)
Parameters: basePointY (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
BasePointZ¶
-
InspectionPlaneFeatureBuilder.
BasePointZ
¶ Returns or sets the base point or plane center Z coordinate
-------------------------------------
Getter Method
Signature
BasePointZ()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BasePointZ(basePointZ)
Parameters: basePointZ (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
CsysReferenceType¶
-
InspectionPlaneFeatureBuilder.
CsysReferenceType
¶ Returns or sets the csys reference type
-------------------------------------
Getter Method
Signature
CsysReferenceType()
Returns: Return type: NXOpen.CAM.CamInspectionOperationCsysreferencetypes
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CsysReferenceType(csysReferenceType)
Parameters: csysReferenceType ( NXOpen.CAM.CamInspectionOperationCsysreferencetypes
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ExtentType¶
-
InspectionPlaneFeatureBuilder.
ExtentType
¶ Returns or sets the extent type
-------------------------------------
Getter Method
Signature
ExtentType()
Returns: Return type: NXOpen.CAM.CamInspectionOperationExtenttypes
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ExtentType(extentType)
Parameters: extentType ( NXOpen.CAM.CamInspectionOperationExtenttypes
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Name¶
-
InspectionPlaneFeatureBuilder.
Name
¶ Returns or sets the plane inspection feature name
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Name(name)
Parameters: name (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
NormalVector¶
-
InspectionPlaneFeatureBuilder.
NormalVector
¶ Returns or sets the normal vector
-------------------------------------
Getter Method
Signature
NormalVector()
Returns: Return type: NXOpen.Direction
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NormalVector(normalVector)
Parameters: normalVector ( NXOpen.Direction
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
NormalVectorI¶
-
InspectionPlaneFeatureBuilder.
NormalVectorI
¶ Returns or sets the normal vector I component
-------------------------------------
Getter Method
Signature
NormalVectorI()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NormalVectorI(normalVectorI)
Parameters: normalVectorI (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
NormalVectorJ¶
-
InspectionPlaneFeatureBuilder.
NormalVectorJ
¶ Returns or sets the normal vector J component
-------------------------------------
Getter Method
Signature
NormalVectorJ()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NormalVectorJ(normalVectorJ)
Parameters: normalVectorJ (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
NormalVectorK¶
-
InspectionPlaneFeatureBuilder.
NormalVectorK
¶ Returns or sets the normal vector K component
-------------------------------------
Getter Method
Signature
NormalVectorK()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NormalVectorK(normalVectorK)
Parameters: normalVectorK (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ReverseFaceNormal¶
-
InspectionPlaneFeatureBuilder.
ReverseFaceNormal
¶ Returns or sets the reverse face normal flag
-------------------------------------
Getter Method
Signature
ReverseFaceNormal()
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReverseFaceNormal(reverseFaceNormal)
Parameters: reverseFaceNormal (bool) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
SelectedPlane¶
-
InspectionPlaneFeatureBuilder.
SelectedPlane
¶ Returns the selected plane
-------------------------------------
Getter Method
Signature
SelectedPlane()
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX7.0.0.
License requirements: None.
Method Detail¶
FlipNormal¶
-
InspectionPlaneFeatureBuilder.
FlipNormal
¶ Flips the plane inspection feature normal vector
Signature
FlipNormal()
New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
UpdateNormalVector¶
-
InspectionPlaneFeatureBuilder.
UpdateNormalVector
¶ Updates plane inspection feature normal vector based on selected vector
Signature
UpdateNormalVector(vector)
Parameters: vector ( NXOpen.Vector3d
) – New normalNew in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
UpdateParams¶
-
InspectionPlaneFeatureBuilder.
UpdateParams
¶ Updates plane inspection feature characteristic parameters based on selected geometry
Signature
UpdateParams()
New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Validate¶
-
InspectionPlaneFeatureBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.