InspectionParplnFeatureBuilder Class¶
-
class
NXOpen.CAM.
InspectionParplnFeatureBuilder
¶ Bases:
NXOpen.CAM.OperationBuilder
Represents a CMM Inspection Parpln Feature Builder.
A Parpln is an unbounded slot or tab defined by two parallel planes. To create a new instance of this class, use
NXOpen.CAM.InspectionOperationCollection.CreateInspectionParplnFeatureBuilder
New in version NX7.0.0.
Properties¶
Property | Description |
---|---|
ChannelName | Returns or sets the channel’s name |
CsysReferenceType | Returns or sets the coordinate system reference type |
CycleEvent | Returns the cycle event |
CycleTable | Returns the cycle |
Description | Returns or sets the description |
EndOfPath | Returns the end event builder |
EndUdeSet | Returns the end ude set |
ExtentType | Returns or sets the extent type of the slot/tab (bounded or unbounded) |
Geometry | Returns the geometry builder |
GougeChecking | Returns or sets the gouge checking flag |
HoleAxisType | Returns or sets the Hole Axis Type |
HoleDepth | Returns the max depth distance builder |
HoleDepthType | Returns or sets the Hole Depth Type |
InnerOuterType | Returns or sets the inspection feature inner outer type (slot/tab) |
LayoutAndLayer | Returns the Layer and Layout |
MotionOutputBuilder | Returns the motion output builder |
Name | Returns or sets the name of the parpln feature |
Notes | Returns the notes builder |
OptimizationBasedOn | Returns or sets the optimization based on in operation |
OptimizationDistanceMethod | Returns or sets the optimization distance method in operation |
OptimizationLevel | Returns or sets the optimization level in operation |
OptimizationMethod | Returns or sets the optim method |
PathDisplayOptions | Returns the path display options builder |
RetractDistance | Returns the Retract Distance builder (inheritable double) |
RetractDistanceOnToolAxisChange | Returns the Retract Distance on Tool Axis Change builder (inheritable double) |
SafeClearance | Returns the safe clearance builder |
SelectToolFlag | Returns or sets the user selected tool |
SelectedSide1 | Returns the first selected side of the parpln slot/tab |
SelectedSide2 | Returns the second selected side of the parpln slot/tab |
Side1NormalVectorI | Returns or sets the I component of the normal vector of the plane on the first side of the parpln |
Side1NormalVectorJ | Returns or sets the J component of the normal vector of the plane on the first side of the parpln |
Side1NormalVectorK | Returns or sets the K component of the normal vector of the plane on the first side of the parpln |
Side1PointX | Returns or sets the X coordinate of the center of the plane on the first side of the parpln |
Side1PointY | Returns or sets the Y coordinate of the center of the plane on the first side of the parpln |
Side1PointZ | Returns or sets the Z coordinate of the center of the plane on the first side of the parpln |
Side2NormalVectorI | Returns or sets the I component of the normal vector of the plane on the second side of the parpln |
Side2NormalVectorJ | Returns or sets the J component of the normal vector of the plane on the second side of the parpln |
Side2NormalVectorK | Returns or sets the K component of the normal vector of the plane on the second side of the parpln |
Side2PointX | Returns or sets the X coordinate of the center of the plane on the second side of the parpln |
Side2PointY | Returns or sets the Y coordinate of the center of the plane on the second side of the parpln |
Side2PointZ | Returns or sets the Z coordinate of the center of the plane on the second side of the parpln |
StartOfPath | Returns the start event builder |
StartUdeSet | Returns the start ude set |
Tag | Returns the Tag for this object. |
ToolChangeSetting | Returns the tool change builder |
ToolPathSplitParametersBuilder | Returns the tool path split Parameters |
Width | Returns or sets the width of the parpln slot/tab |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetHoleAxisValues | Get the Hole Axis values @return the Hole Axis values |
GetObject | Returns the object currently being edited by this builder. |
SetHoleAxisValues | Set the Hole Axis values |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UpdateParams | Updates parpln inspection feature characteristic parameters based on selected geometry |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
CsysReferenceType¶
-
InspectionParplnFeatureBuilder.
CsysReferenceType
¶ Returns or sets the coordinate system reference type
-------------------------------------
Getter Method
Signature
CsysReferenceType()
Returns: Return type: NXOpen.CAM.CamInspectionOperationCsysreferencetypes
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CsysReferenceType(csysReferenceType)
Parameters: csysReferenceType ( NXOpen.CAM.CamInspectionOperationCsysreferencetypes
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ExtentType¶
-
InspectionParplnFeatureBuilder.
ExtentType
¶ Returns or sets the extent type of the slot/tab (bounded or unbounded)
-------------------------------------
Getter Method
Signature
ExtentType()
Returns: Return type: NXOpen.CAM.CamInspectionOperationExtenttypes
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ExtentType(extentType)
Parameters: extentType ( NXOpen.CAM.CamInspectionOperationExtenttypes
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
InnerOuterType¶
-
InspectionParplnFeatureBuilder.
InnerOuterType
¶ Returns or sets the inspection feature inner outer type (slot/tab)
-------------------------------------
Getter Method
Signature
InnerOuterType()
Returns: Return type: NXOpen.CAM.CamInspectionOperationInneroutertypes
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InnerOuterType(innerOuterType)
Parameters: innerOuterType ( NXOpen.CAM.CamInspectionOperationInneroutertypes
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Name¶
-
InspectionParplnFeatureBuilder.
Name
¶ Returns or sets the name of the parpln feature
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Name(name)
Parameters: name (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
SelectedSide1¶
-
InspectionParplnFeatureBuilder.
SelectedSide1
¶ Returns the first selected side of the parpln slot/tab
-------------------------------------
Getter Method
Signature
SelectedSide1()
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX7.0.0.
License requirements: None.
SelectedSide2¶
-
InspectionParplnFeatureBuilder.
SelectedSide2
¶ Returns the second selected side of the parpln slot/tab
-------------------------------------
Getter Method
Signature
SelectedSide2()
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX7.0.0.
License requirements: None.
Side1NormalVectorI¶
-
InspectionParplnFeatureBuilder.
Side1NormalVectorI
¶ Returns or sets the I component of the normal vector of the plane on the first side of the parpln
-------------------------------------
Getter Method
Signature
Side1NormalVectorI()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Side1NormalVectorI(side1NormalVectorI)
Parameters: side1NormalVectorI (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Side1NormalVectorJ¶
-
InspectionParplnFeatureBuilder.
Side1NormalVectorJ
¶ Returns or sets the J component of the normal vector of the plane on the first side of the parpln
-------------------------------------
Getter Method
Signature
Side1NormalVectorJ()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Side1NormalVectorJ(side1NormalVectorJ)
Parameters: side1NormalVectorJ (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Side1NormalVectorK¶
-
InspectionParplnFeatureBuilder.
Side1NormalVectorK
¶ Returns or sets the K component of the normal vector of the plane on the first side of the parpln
-------------------------------------
Getter Method
Signature
Side1NormalVectorK()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Side1NormalVectorK(side1NormalVectorK)
Parameters: side1NormalVectorK (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Side1PointX¶
-
InspectionParplnFeatureBuilder.
Side1PointX
¶ Returns or sets the X coordinate of the center of the plane on the first side of the parpln
-------------------------------------
Getter Method
Signature
Side1PointX()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Side1PointX(side1PointX)
Parameters: side1PointX (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Side1PointY¶
-
InspectionParplnFeatureBuilder.
Side1PointY
¶ Returns or sets the Y coordinate of the center of the plane on the first side of the parpln
-------------------------------------
Getter Method
Signature
Side1PointY()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Side1PointY(side1PointY)
Parameters: side1PointY (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Side1PointZ¶
-
InspectionParplnFeatureBuilder.
Side1PointZ
¶ Returns or sets the Z coordinate of the center of the plane on the first side of the parpln
-------------------------------------
Getter Method
Signature
Side1PointZ()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Side1PointZ(side1PointZ)
Parameters: side1PointZ (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Side2NormalVectorI¶
-
InspectionParplnFeatureBuilder.
Side2NormalVectorI
¶ Returns or sets the I component of the normal vector of the plane on the second side of the parpln
-------------------------------------
Getter Method
Signature
Side2NormalVectorI()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Side2NormalVectorI(side2NormalVectorI)
Parameters: side2NormalVectorI (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Side2NormalVectorJ¶
-
InspectionParplnFeatureBuilder.
Side2NormalVectorJ
¶ Returns or sets the J component of the normal vector of the plane on the second side of the parpln
-------------------------------------
Getter Method
Signature
Side2NormalVectorJ()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Side2NormalVectorJ(side2NormalVectorJ)
Parameters: side2NormalVectorJ (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Side2NormalVectorK¶
-
InspectionParplnFeatureBuilder.
Side2NormalVectorK
¶ Returns or sets the K component of the normal vector of the plane on the second side of the parpln
-------------------------------------
Getter Method
Signature
Side2NormalVectorK()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Side2NormalVectorK(side2NormalVectorK)
Parameters: side2NormalVectorK (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Side2PointX¶
-
InspectionParplnFeatureBuilder.
Side2PointX
¶ Returns or sets the X coordinate of the center of the plane on the second side of the parpln
-------------------------------------
Getter Method
Signature
Side2PointX()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Side2PointX(side2PointX)
Parameters: side2PointX (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Side2PointY¶
-
InspectionParplnFeatureBuilder.
Side2PointY
¶ Returns or sets the Y coordinate of the center of the plane on the second side of the parpln
-------------------------------------
Getter Method
Signature
Side2PointY()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Side2PointY(side2PointY)
Parameters: side2PointY (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Side2PointZ¶
-
InspectionParplnFeatureBuilder.
Side2PointZ
¶ Returns or sets the Z coordinate of the center of the plane on the second side of the parpln
-------------------------------------
Getter Method
Signature
Side2PointZ()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Side2PointZ(side2PointZ)
Parameters: side2PointZ (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Width¶
-
InspectionParplnFeatureBuilder.
Width
¶ Returns or sets the width of the parpln slot/tab
-------------------------------------
Getter Method
Signature
Width()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Width(width)
Parameters: width (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Method Detail¶
UpdateParams¶
-
InspectionParplnFeatureBuilder.
UpdateParams
¶ Updates parpln inspection feature characteristic parameters based on selected geometry
Signature
UpdateParams()
New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Validate¶
-
InspectionParplnFeatureBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.