InspectionOutputOperationBuilder Class¶
-
class
NXOpen.CAM.
InspectionOutputOperationBuilder
¶ Bases:
NXOpen.CAM.OperationBuilder
this class creates the output operation
To create a new instance of this class, use
NXOpen.CAM.InspectionOperationCollection.CreateInspectionOutputOperationBuilder
New in version NX7.0.0.
Properties¶
Property | Description |
---|---|
ChannelName | Returns or sets the channel’s name |
CycleEvent | Returns the cycle event |
CycleTable | Returns the cycle |
Description | Returns or sets the description |
EndOfPath | Returns the end event builder |
EndUdeSet | Returns the end ude set |
EnumTypeOutput | Returns or sets the enum type output |
Geometry | Returns the geometry builder |
GougeChecking | Returns or sets the gouge checking flag |
HoleAxisType | Returns or sets the Hole Axis Type |
HoleDepth | Returns the max depth distance builder |
HoleDepthType | Returns or sets the Hole Depth Type |
LayoutAndLayer | Returns the Layer and Layout |
MotionOutputBuilder | Returns the motion output builder |
Notes | Returns the notes builder |
OptimizationBasedOn | Returns or sets the optimization based on in operation |
OptimizationDistanceMethod | Returns or sets the optimization distance method in operation |
OptimizationLevel | Returns or sets the optimization level in operation |
OptimizationMethod | Returns or sets the optim method |
PathDisplayOptions | Returns the path display options builder |
RetractDistance | Returns the Retract Distance builder (inheritable double) |
RetractDistanceOnToolAxisChange | Returns the Retract Distance on Tool Axis Change builder (inheritable double) |
SafeClearance | Returns the safe clearance builder |
SelectToolFlag | Returns or sets the user selected tool |
StartOfPath | Returns the start event builder |
StartUdeSet | Returns the start ude set |
StringFeatureName1 | Returns or sets the string feature name1 |
StringFeatureName2 | Returns or sets the string feature name2 |
StringTolName | Returns or sets the string tol name |
Tag | Returns the Tag for this object. |
ToolChangeSetting | Returns the tool change builder |
ToolPathSplitParametersBuilder | Returns the tool path split Parameters |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetHoleAxisValues | Get the Hole Axis values @return the Hole Axis values |
GetObject | Returns the object currently being edited by this builder. |
SetHoleAxisValues | Set the Hole Axis values |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
InspectionOutputOperationBuilderTypeOutput Enumeration | Represents the output operation types |
Property Detail¶
EnumTypeOutput¶
-
InspectionOutputOperationBuilder.
EnumTypeOutput
¶ Returns or sets the enum type output
-------------------------------------
Getter Method
Signature
EnumTypeOutput()
Returns: Return type: NXOpen.CAM.InspectionOutputOperationBuilderTypeOutput
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EnumTypeOutput(enumTypeOutput)
Parameters: enumTypeOutput ( NXOpen.CAM.InspectionOutputOperationBuilderTypeOutput
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
StringFeatureName1¶
-
InspectionOutputOperationBuilder.
StringFeatureName1
¶ Returns or sets the string feature name1
-------------------------------------
Getter Method
Signature
StringFeatureName1()
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StringFeatureName1(stringFeatureName1)
Parameters: stringFeatureName1 (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
StringFeatureName2¶
-
InspectionOutputOperationBuilder.
StringFeatureName2
¶ Returns or sets the string feature name2
-------------------------------------
Getter Method
Signature
StringFeatureName2()
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StringFeatureName2(stringFeatureName2)
Parameters: stringFeatureName2 (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
StringTolName¶
-
InspectionOutputOperationBuilder.
StringTolName
¶ Returns or sets the string tol name
-------------------------------------
Getter Method
Signature
StringTolName()
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StringTolName(stringTolName)
Parameters: stringTolName (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Method Detail¶
Validate¶
-
InspectionOutputOperationBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.