InspectionOperationTransformBuilderAngle Enumeration¶
NXOpen.CAM.InspectionOperationTransformBuilder.Angle is an alias for NXOpen.CAM.InspectionOperationTransformBuilderAngle
-
class
NXOpen.CAM.
InspectionOperationTransformBuilderAngle
¶ Bases:
object
Angle Type
Enum Members
Enum Member Enum Member Description Specify specify a angleTwoPoint use two point to sepcify a angle-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-