InspectionMethodBuilderOperationTypes Enumeration¶
NXOpen.CAM.InspectionMethodBuilder.OperationTypes is an alias for NXOpen.CAM.InspectionMethodBuilderOperationTypes
-
class
NXOpen.CAM.
InspectionMethodBuilderOperationTypes
¶ Bases:
object
CMM Inspection operation types.
Enum Members
Enum Member Enum Member Description None NoneManualPoint Measured PointUVGrid Point Set (Rectangular UV Grid)PointHelix Point HelixLineScan Scan LineCircularScan Scan ArcCurveScan Scan CurveHelicalScan Scan HelixCurveScan5axis 5-axis Scan CurveLinearSafeMoveToPoint Linear Safe Move To PointDeltaMove Delta MoveLinear5axisMoveToPoint Linear 5-axis Move To Point-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-