InspectionMethodBuilderMethodTypes Enumeration¶
NXOpen.CAM.InspectionMethodBuilder.MethodTypes is an alias for NXOpen.CAM.InspectionMethodBuilderMethodTypes
-
class
NXOpen.CAM.
InspectionMethodBuilderMethodTypes
¶ Bases:
object
CMM Inspection method feature type.
Enum Members
Enum Member Enum Member Description None NoneArc ArcCircle CirclePoint PointSphere SphereSurface SurfacePattern PatternCurve CurveCylinder CylinderCone ConePlane PlaneLine LineCParln Bounded Slot TabSlotTab Slot TabSurfaceOfRevolution Surface of RevolutionTorus TorusEdgePt Edge Point-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-