InspectionMeasurePointBuilder Class¶
-
class
NXOpen.CAM.
InspectionMeasurePointBuilder
¶ Bases:
NXOpen.CAM.InspectionMoveBuilder
Represents the builder for the CMM Inspection sub-operation Measure Point.
To create a new instance of this class, use
NXOpen.CAM.InspectionMoveCollection.CreateInspectionMeasurePointBuilder
New in version NX7.0.0.
Properties¶
Property | Description |
---|---|
AngleA | Returns or sets the A angle for an indexable head |
AngleB | Returns or sets the B angle for an indexable head |
ApproachDist | Returns the builder for approach distance |
ApproachDistance | Returns or sets the approach distance |
DepthDistance | Returns or sets the depth distance |
DepthMethod | Returns or sets the depth method |
NXOpen.CAM.InspectionMeasurePointBuilder.I | Returns or sets the I direction at measured point |
NXOpen.CAM.InspectionMeasurePointBuilder.J | Returns or sets the J direction at measured point |
NXOpen.CAM.InspectionMeasurePointBuilder.K | Returns or sets the K direction at measured point |
MotionType | Returns or sets the motion type |
PointTypeEnum | Returns or sets the point type enum |
ProbeTipType | Returns or sets the preferred probe tip type |
ProbeTipTypeBuilder | Returns the Probe Tip Type Builder |
RetractDist | Returns the builder for retract distance |
RetractDistance | Returns or sets the retract distance |
SelectExistingPoint | Returns the select existing point |
SensorOpName | Returns or sets the inspection sensor operation name |
SensorStrategy | Returns or sets the sensor selection strategy |
SensorStrategyBuilder | Returns the Sensor Strategy Enum Builder |
Tag | Returns the Tag for this object. |
TargetPoint | Returns or sets the point |
TipAngleMode | Returns or sets the tip angle selection mode |
TipMode | Returns or sets the probe tip selection mode |
TipNumber | Returns or sets the probe tip number |
NXOpen.CAM.InspectionMeasurePointBuilder.X | Returns or sets the X at measured point |
NXOpen.CAM.InspectionMeasurePointBuilder.Y | Returns or sets the Y at measured point |
NXOpen.CAM.InspectionMeasurePointBuilder.Z | Returns or sets the Z at measured point |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SetParent | Set parent |
SetProbeAngles | Set default values for probe angles based on feature type. |
SetProbeTip | Set default probe tip based on preferred tip type and probe angles. |
SetSibling | Set sibling |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UpdateParams | Update measured point parameters based on selected point. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
InspectionMeasurePointBuilderPointTypes Enumeration | specifies the method used to define a point |
Property Detail¶
ApproachDist¶
-
InspectionMeasurePointBuilder.
ApproachDist
¶ Returns the builder for approach distance
-------------------------------------
Getter Method
Signature
ApproachDist()
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX9.0.2.
License requirements: None.
DepthDistance¶
-
InspectionMeasurePointBuilder.
DepthDistance
¶ Returns or sets the depth distance
-------------------------------------
Getter Method
Signature
DepthDistance()
Returns: Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DepthDistance(distance)
Parameters: distance (float) – New in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
DepthMethod¶
-
InspectionMeasurePointBuilder.
DepthMethod
¶ Returns or sets the depth method
-------------------------------------
Getter Method
Signature
DepthMethod()
Returns: Return type: NXOpen.CAM.InspectionMoveBuilderDepthMethodTypes
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DepthMethod(method)
Parameters: method ( NXOpen.CAM.InspectionMoveBuilderDepthMethodTypes
) –New in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
I¶
-
InspectionMeasurePointBuilder.
I
¶ Returns or sets the I direction at measured point
-------------------------------------
Getter Method
Signature
I()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
I(direction)
Parameters: direction (float) – New in version NX7.0.0.
License requirements: None.
J¶
-
InspectionMeasurePointBuilder.
J
¶ Returns or sets the J direction at measured point
-------------------------------------
Getter Method
Signature
J()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
J(direction)
Parameters: direction (float) – New in version NX7.0.0.
License requirements: None.
K¶
-
InspectionMeasurePointBuilder.
K
¶ Returns or sets the K direction at measured point
-------------------------------------
Getter Method
Signature
K()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
K(direction)
Parameters: direction (float) – New in version NX7.0.0.
License requirements: None.
PointTypeEnum¶
-
InspectionMeasurePointBuilder.
PointTypeEnum
¶ Returns or sets the point type enum
-------------------------------------
Getter Method
Signature
PointTypeEnum()
Returns: Return type: NXOpen.CAM.InspectionMeasurePointBuilderPointTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PointTypeEnum(pointTypeEnum)
Parameters: pointTypeEnum ( NXOpen.CAM.InspectionMeasurePointBuilderPointTypes
) –New in version NX7.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
RetractDist¶
-
InspectionMeasurePointBuilder.
RetractDist
¶ Returns the builder for retract distance
-------------------------------------
Getter Method
Signature
RetractDist()
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX9.0.2.
License requirements: None.
SelectExistingPoint¶
-
InspectionMeasurePointBuilder.
SelectExistingPoint
¶ Returns the select existing point
-------------------------------------
Getter Method
Signature
SelectExistingPoint()
Returns: Return type: NXOpen.SelectPoint
New in version NX7.5.0.
License requirements: None.
TargetPoint¶
-
InspectionMeasurePointBuilder.
TargetPoint
¶ Returns or sets the point
-------------------------------------
Getter Method
Signature
TargetPoint()
Returns: Return type: NXOpen.Point
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TargetPoint(point)
Parameters: point ( NXOpen.Point
) –New in version NX7.0.0.
License requirements: None.
X¶
-
InspectionMeasurePointBuilder.
X
¶ Returns or sets the X at measured point
-------------------------------------
Getter Method
Signature
X()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
X(x)
Parameters: x (float) – New in version NX7.0.0.
License requirements: None.
Y¶
-
InspectionMeasurePointBuilder.
Y
¶ Returns or sets the Y at measured point
-------------------------------------
Getter Method
Signature
Y()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Y(y)
Parameters: y (float) – New in version NX7.0.0.
License requirements: None.
Z¶
-
InspectionMeasurePointBuilder.
Z
¶ Returns or sets the Z at measured point
-------------------------------------
Getter Method
Signature
Z()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Z(z)
Parameters: z (float) – New in version NX7.0.0.
License requirements: None.
Method Detail¶
UpdateParams¶
-
InspectionMeasurePointBuilder.
UpdateParams
¶ Update measured point parameters based on selected point.
Signature
UpdateParams()
New in version NX7.5.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Validate¶
-
InspectionMeasurePointBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.