InspectionMeasDataBuilder Class¶
-
class
NXOpen.CAM.
InspectionMeasDataBuilder
¶ Bases:
NXOpen.Builder
Inspection Measured Data dialog builder
To create a new instance of this class, use
NXOpen.CAM.InspectionOperationCollection.CreateInspectionMeasDataBuilder
New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
DisplayTransform | Returns or sets the display transform |
FeatDisplayDesPoints | Returns or sets the option to display design points for a feature |
FeatDisplayMeaPoints | Returns or sets the option to display measured points for a feature |
FeatDisplayReconstruct | Returns or sets the option to display the reconstructed feature |
FeatHighlightNominal | Returns or sets the option to highlight nominal faces for a feature |
HolePinMatching | Returns or sets the hole pin matching mode when adding measured data |
InputFormat | Returns or sets the measured data input file format |
Layer | Returns or sets the layer to save results to |
MeaFile | Returns or sets the measured data file |
NeedleScale | Returns or sets the needles scale factor |
OffsetDist | Returns or sets the offset distance when adding measured data |
PcsName | Returns or sets the name of the PCS to use when transforming data being loaded |
ProjectLimit | Returns or sets the projection limit when adding measured data |
Tag | Returns the Tag for this object. |
TolDisplayActDRF | Returns or sets the option to display the tolerance actual DRF (datum reference frame) |
TolDisplayDesDRF | Returns or sets the option to display the tolerance design DRF (datum reference frame) |
TolDisplayDesPoints | Returns or sets the option to display design points for the features of a tolerance |
TolDisplayGauge | Returns or sets the option to display the gauge in position for a tolerance |
TolDisplayMeaPoints | Returns or sets the option to display measured points for the features of a tolerance |
TolDisplayNeedles | Returns or sets the option to display tolerance deviation needles |
TolDisplayPoints | Returns or sets the option to display points in position for a tolerance |
TolDisplayReconstruct | Returns or sets the option to display the reconstructed features of a tolerance |
TolHighlightNominal | Returns or sets the option to highlight nominal faces for a tolerance |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
LoadMea | Load measured data file |
SaveToLayer | Save results to layer |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnloadMea | Unload measured data file |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
InspectionMeasDataBuilderBoundingType Enumeration | Hole/Pin Matching Mode |
InspectionMeasDataBuilderDisplayTransformTypes Enumeration | Transform Display Types |
InspectionMeasDataBuilderInputFormatType Enumeration | Measured Data Input File Format Types |
Property Detail¶
DisplayTransform¶
-
InspectionMeasDataBuilder.
DisplayTransform
¶ Returns or sets the display transform
-------------------------------------
Getter Method
Signature
DisplayTransform()
Returns: Return type: NXOpen.CAM.InspectionMeasDataBuilderDisplayTransformTypes
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DisplayTransform(displayTransform)
Parameters: displayTransform ( NXOpen.CAM.InspectionMeasDataBuilderDisplayTransformTypes
) –New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
FeatDisplayDesPoints¶
-
InspectionMeasDataBuilder.
FeatDisplayDesPoints
¶ Returns or sets the option to display design points for a feature
-------------------------------------
Getter Method
Signature
FeatDisplayDesPoints()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FeatDisplayDesPoints(featDisplayDesPoints)
Parameters: featDisplayDesPoints (bool) – New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
FeatDisplayMeaPoints¶
-
InspectionMeasDataBuilder.
FeatDisplayMeaPoints
¶ Returns or sets the option to display measured points for a feature
-------------------------------------
Getter Method
Signature
FeatDisplayMeaPoints()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FeatDisplayMeaPoints(featDisplayMeaPoints)
Parameters: featDisplayMeaPoints (bool) – New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
FeatDisplayReconstruct¶
-
InspectionMeasDataBuilder.
FeatDisplayReconstruct
¶ Returns or sets the option to display the reconstructed feature
-------------------------------------
Getter Method
Signature
FeatDisplayReconstruct()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FeatDisplayReconstruct(featDisplayReconstruct)
Parameters: featDisplayReconstruct (bool) – New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
FeatHighlightNominal¶
-
InspectionMeasDataBuilder.
FeatHighlightNominal
¶ Returns or sets the option to highlight nominal faces for a feature
-------------------------------------
Getter Method
Signature
FeatHighlightNominal()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FeatHighlightNominal(featHighlightNominal)
Parameters: featHighlightNominal (bool) – New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
HolePinMatching¶
-
InspectionMeasDataBuilder.
HolePinMatching
¶ Returns or sets the hole pin matching mode when adding measured data
-------------------------------------
Getter Method
Signature
HolePinMatching()
Returns: Return type: NXOpen.CAM.InspectionMeasDataBuilderBoundingType
New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
HolePinMatching(holePinMatching)
Parameters: holePinMatching ( NXOpen.CAM.InspectionMeasDataBuilderBoundingType
) –New in version NX8.5.1.
License requirements: None.
InputFormat¶
-
InspectionMeasDataBuilder.
InputFormat
¶ Returns or sets the measured data input file format
-------------------------------------
Getter Method
Signature
InputFormat()
Returns: Return type: NXOpen.CAM.InspectionMeasDataBuilderInputFormatType
New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
InputFormat(inputFormat)
Parameters: inputFormat ( NXOpen.CAM.InspectionMeasDataBuilderInputFormatType
) –New in version NX8.5.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Layer¶
-
InspectionMeasDataBuilder.
Layer
¶ Returns or sets the layer to save results to
-------------------------------------
Getter Method
Signature
Layer()
Returns: Return type: int New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
Layer(layer)
Parameters: layer (int) – New in version NX8.5.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
MeaFile¶
-
InspectionMeasDataBuilder.
MeaFile
¶ Returns or sets the measured data file
-------------------------------------
Getter Method
Signature
MeaFile()
Returns: Return type: str New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MeaFile(filename)
Parameters: filename (str) – New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
NeedleScale¶
-
InspectionMeasDataBuilder.
NeedleScale
¶ Returns or sets the needles scale factor
-------------------------------------
Getter Method
Signature
NeedleScale()
Returns: Return type: float New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
NeedleScale(needleScale)
Parameters: needleScale (float) – New in version NX8.5.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
OffsetDist¶
-
InspectionMeasDataBuilder.
OffsetDist
¶ Returns or sets the offset distance when adding measured data
-------------------------------------
Getter Method
Signature
OffsetDist()
Returns: Return type: float New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
OffsetDist(offsetDist)
Parameters: offsetDist (float) – New in version NX8.5.1.
License requirements: None.
PcsName¶
-
InspectionMeasDataBuilder.
PcsName
¶ Returns or sets the name of the PCS to use when transforming data being loaded
-------------------------------------
Getter Method
Signature
PcsName()
Returns: Return type: str New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PcsName(pcsName)
Parameters: pcsName (str) – New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ProjectLimit¶
-
InspectionMeasDataBuilder.
ProjectLimit
¶ Returns or sets the projection limit when adding measured data
-------------------------------------
Getter Method
Signature
ProjectLimit()
Returns: Return type: float New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
ProjectLimit(projectLimit)
Parameters: projectLimit (float) – New in version NX8.5.1.
License requirements: None.
TolDisplayActDRF¶
-
InspectionMeasDataBuilder.
TolDisplayActDRF
¶ Returns or sets the option to display the tolerance actual DRF (datum reference frame)
-------------------------------------
Getter Method
Signature
TolDisplayActDRF()
Returns: Return type: bool New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
TolDisplayActDRF(tolDisplayDRF)
Parameters: tolDisplayDRF (bool) – New in version NX8.5.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
TolDisplayDesDRF¶
-
InspectionMeasDataBuilder.
TolDisplayDesDRF
¶ Returns or sets the option to display the tolerance design DRF (datum reference frame)
-------------------------------------
Getter Method
Signature
TolDisplayDesDRF()
Returns: Return type: bool New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
TolDisplayDesDRF(tolDisplayDRF)
Parameters: tolDisplayDRF (bool) – New in version NX8.5.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
TolDisplayDesPoints¶
-
InspectionMeasDataBuilder.
TolDisplayDesPoints
¶ Returns or sets the option to display design points for the features of a tolerance
-------------------------------------
Getter Method
Signature
TolDisplayDesPoints()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TolDisplayDesPoints(tolDisplayDesPoints)
Parameters: tolDisplayDesPoints (bool) – New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
TolDisplayGauge¶
-
InspectionMeasDataBuilder.
TolDisplayGauge
¶ Returns or sets the option to display the gauge in position for a tolerance
-------------------------------------
Getter Method
Signature
TolDisplayGauge()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TolDisplayGauge(tolDisplayGauge)
Parameters: tolDisplayGauge (bool) – New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
TolDisplayMeaPoints¶
-
InspectionMeasDataBuilder.
TolDisplayMeaPoints
¶ Returns or sets the option to display measured points for the features of a tolerance
-------------------------------------
Getter Method
Signature
TolDisplayMeaPoints()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TolDisplayMeaPoints(tolDisplayMeaPoints)
Parameters: tolDisplayMeaPoints (bool) – New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
TolDisplayNeedles¶
-
InspectionMeasDataBuilder.
TolDisplayNeedles
¶ Returns or sets the option to display tolerance deviation needles
-------------------------------------
Getter Method
Signature
TolDisplayNeedles()
Returns: Return type: bool New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
TolDisplayNeedles(tolDisplayNeedles)
Parameters: tolDisplayNeedles (bool) – New in version NX8.5.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
TolDisplayPoints¶
-
InspectionMeasDataBuilder.
TolDisplayPoints
¶ Returns or sets the option to display points in position for a tolerance
-------------------------------------
Getter Method
Signature
TolDisplayPoints()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TolDisplayPoints(tolDisplayPoints)
Parameters: tolDisplayPoints (bool) – New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
TolDisplayReconstruct¶
-
InspectionMeasDataBuilder.
TolDisplayReconstruct
¶ Returns or sets the option to display the reconstructed features of a tolerance
-------------------------------------
Getter Method
Signature
TolDisplayReconstruct()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TolDisplayReconstruct(tolDisplayReconstruct)
Parameters: tolDisplayReconstruct (bool) – New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
TolHighlightNominal¶
-
InspectionMeasDataBuilder.
TolHighlightNominal
¶ Returns or sets the option to highlight nominal faces for a tolerance
-------------------------------------
Getter Method
Signature
TolHighlightNominal()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TolHighlightNominal(tolHighlightNominal)
Parameters: tolHighlightNominal (bool) – New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Method Detail¶
LoadMea¶
-
InspectionMeasDataBuilder.
LoadMea
¶ Load measured data file
Signature
LoadMea()
New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
SaveToLayer¶
-
InspectionMeasDataBuilder.
SaveToLayer
¶ Save results to layer
Signature
SaveToLayer()
New in version NX8.5.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
UnloadMea¶
-
InspectionMeasDataBuilder.
UnloadMea
¶ Unload measured data file
Signature
UnloadMea()
New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Validate¶
-
InspectionMeasDataBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.