InspectionLinkPmiBuilderPmiScopeTypes Enumeration¶
NXOpen.CAM.InspectionLinkPmiBuilder.PmiScopeTypes is an alias for NXOpen.CAM.InspectionLinkPmiBuilderPmiScopeTypes
-
class
NXOpen.CAM.
InspectionLinkPmiBuilderPmiScopeTypes
¶ Bases:
object
Specifies the scope of the link PMI command
Enum Members
Enum Member Enum Member Description WorkpieceOnly Link PMI will be performed for the workpiece onlyWorkpieceandComponents Link PMI will be performed for the workpiece and components-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-